InspectionCmmCommandBuilderIdnameMethods Enumeration

NXOpen.CAM.InspectionCmmCommandBuilder.IdnameMethods is an alias for NXOpen.CAM.InspectionCmmCommandBuilderIdnameMethods

class NXOpen.CAM.InspectionCmmCommandBuilderIdnameMethods

Bases: object

Naming method

Enum Members

Enum Member Enum Member Description
CurrentPartName
Use current part name for ID
UserSpecified
Use user specified name for ID
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.