InspectionCmmCommandBuilderHomePtMethods Enumeration¶
NXOpen.CAM.InspectionCmmCommandBuilder.HomePtMethods is an alias for NXOpen.CAM.InspectionCmmCommandBuilderHomePtMethods
-
class
NXOpen.CAM.
InspectionCmmCommandBuilderHomePtMethods
¶ Bases:
object
The method used to specify the home point
Enum Members
Enum Member Enum Member Description MachineZero Use the Machine zero point as the home pointUserSpecifiedPoint Use a user specified point as the home point-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-