InspectionCmmCommandBuilderAngularUnitsOptions Enumeration

NXOpen.CAM.InspectionCmmCommandBuilder.AngularUnitsOptions is an alias for NXOpen.CAM.InspectionCmmCommandBuilderAngularUnitsOptions

class NXOpen.CAM.InspectionCmmCommandBuilderAngularUnitsOptions

Bases: object

Angular units specifications

Enum Members

Enum Member Enum Member Description
DecimalDegrees
Use decimal degrees
Radians
Use radians
DegreesMinutesSeconds
Use Degrees:Minutes:Seconds
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.