InspectionCmmCommandBuilderRevMethods Enumeration

NXOpen.CAM.InspectionCmmCommandBuilder.RevMethods is an alias for NXOpen.CAM.InspectionCmmCommandBuilderRevMethods

class NXOpen.CAM.InspectionCmmCommandBuilderRevMethods

Bases: object

Revision method

Enum Members

Enum Member Enum Member Description
CurrentPartRevision
Use current part revision
UserSpecified
Use user specified revision
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.