InspectionCmmCommandBuilderVarTypes Enumeration

NXOpen.CAM.InspectionCmmCommandBuilder.VarTypes is an alias for NXOpen.CAM.InspectionCmmCommandBuilderVarTypes

class NXOpen.CAM.InspectionCmmCommandBuilderVarTypes

Bases: object

Variable type

Enum Members

Enum Member Enum Member Description
Boolean
Specifies a boolean variable
Integer
Specifies an integer variable
Long
Specifies a long integer variable
Real
Specifies a real variable
Double
Specifies a double variable
Character
Specifies a character variable
Vector
Specifies a vector variable
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.