InspectionCmmCommandBuilderTemperatureUnitsOptions Enumeration

NXOpen.CAM.InspectionCmmCommandBuilder.TemperatureUnitsOptions is an alias for NXOpen.CAM.InspectionCmmCommandBuilderTemperatureUnitsOptions

class NXOpen.CAM.InspectionCmmCommandBuilderTemperatureUnitsOptions

Bases: object

Temperature units specifications

Enum Members

Enum Member Enum Member Description
Fahrenheit
Use fahrenheit
Centigrade
Use Centigrade
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.