Package | Description |
---|---|
nxopen.formboard |
Provides interfaces and classes to the Routing Electrical Formboard functionality.
|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Class and Description |
---|
FlipComponentBuilder
Builder for flip component operation used in formboard.
|
FlipComponentBuilder.AxisType
Enum for the selection of axis type for flipping formboard component
|
FormboardLayoutBuilder
Class that performs the "layout" of Formboard geometry.
|
FormboardLayoutBuilder.BranchAngle
Methods for determining which angles to apply at each branch of the Formboard.
|
FormboardLayoutBuilder.BranchShape
Shape option for the branches.
|
FormboardLayoutBuilder.MainRunType
Selection method for the set of segments that define the main
run of the formboard geometry.
|
LayoutLengthOptions
Defines the various options for determining the rounded lengths of
formboard geometry during the layout or update process.
|
LayoutLengthOptions.RoundingMethod
Methods of rounding lengths for Formboard geometry.
|
ObjectAttributeReferenceBuilder
Builder for "object attribute" used in formboard which enbles user to create
annotation in drafting functionality.
|
ObjectAttributeReferenceBuilder.LeaderType
Enum which defines types of leader user wants to associate with the annotation.
|
OrientBranchBuilder
Builder for "Orient Branch" operation used in formboard.
|
OrientBranchBuilder.BranchAngleMethod
Enum to define the type of method to orient branch.
|
ShapeSegmentBuilder
Builder for Face Annotation functionality used in formboard.
|
ShapeSegmentBuilder.LineData
This class holds the data returned from
ShapeSegmentBuilder.getLineData() |
UpdateDiscrepancy
Defines a discrepancy object which contains information about a specific
difference between the formboard drawing and the 3D harness model.
|
UpdateDiscrepancy.ObjectType
Specifies the type of objects involved in the discrepancy.
|
UpdateDiscrepancy.Type
The general type of the discrepancy.
|
UpdateFormboardBuilder
Class that performs the "update" of Formboard geometry.
|
Class and Description |
---|
FormboardManager
Contains information about flattened harness drawing and drafting data for
harness manufacturing drawings (Formboard Drawings).
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.