Package | Description |
---|---|
nxopen.formboard |
Provides interfaces and classes to the Routing Electrical Formboard functionality.
|
Modifier and Type | Field and Description |
---|---|
static FormboardLayoutBuilder.BranchAngle |
FormboardLayoutBuilder.BranchAngle.AS_DESIGNED
Use the angle equal to the 3D angle
of the branch in the 3D harness.
|
static FormboardLayoutBuilder.BranchAngle |
FormboardLayoutBuilder.BranchAngle.MAXIMUM_ANGLES
Apply the largest possible angle values
at every branch to force the harness
to spread out.
|
static FormboardLayoutBuilder.BranchAngle |
FormboardLayoutBuilder.BranchAngle.RANDOM_ANGLES
Randomly choose an angle for each
branch.
|
static FormboardLayoutBuilder.BranchAngle |
FormboardLayoutBuilder.BranchAngle.STANDARD_ANGLES
Apply a standard angle to the branch,
the level of the branch determines
which angle to apply.
|
Modifier and Type | Method and Description |
---|---|
FormboardLayoutBuilder.BranchAngle |
FormboardLayoutBuilder.branchAngleMethod()
Returns the branch angle type.
|
static FormboardLayoutBuilder.BranchAngle |
FormboardLayoutBuilder.BranchAngle.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FormboardLayoutBuilder.BranchAngle |
FormboardLayoutBuilder.BranchAngle.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FormboardLayoutBuilder.BranchAngle[] |
FormboardLayoutBuilder.BranchAngle.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FormboardLayoutBuilder.setBranchAngleMethod(FormboardLayoutBuilder.BranchAngle branchAngle)
License requirements: routing_harness ("Routing Harness") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.