public static class FormboardLayoutBuilder.BranchAngle extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AS_DESIGNED
Use the angle equal to the 3D angle
of the branch in the 3D harness.
|
static int |
_MAXIMUM_ANGLES
Apply the largest possible angle values
at every branch to force the harness
to spread out.
|
static int |
_RANDOM_ANGLES
Randomly choose an angle for each
branch.
|
static int |
_STANDARD_ANGLES
Apply a standard angle to the branch,
the level of the branch determines
which angle to apply.
|
static FormboardLayoutBuilder.BranchAngle |
AS_DESIGNED
Use the angle equal to the 3D angle
of the branch in the 3D harness.
|
static FormboardLayoutBuilder.BranchAngle |
MAXIMUM_ANGLES
Apply the largest possible angle values
at every branch to force the harness
to spread out.
|
static FormboardLayoutBuilder.BranchAngle |
RANDOM_ANGLES
Randomly choose an angle for each
branch.
|
static FormboardLayoutBuilder.BranchAngle |
STANDARD_ANGLES
Apply a standard angle to the branch,
the level of the branch determines
which angle to apply.
|
Modifier and Type | Method and Description |
---|---|
static FormboardLayoutBuilder.BranchAngle |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FormboardLayoutBuilder.BranchAngle |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FormboardLayoutBuilder.BranchAngle[] |
values()
Returns an array that contains the values for this enum.
|
public static final FormboardLayoutBuilder.BranchAngle AS_DESIGNED
public static final FormboardLayoutBuilder.BranchAngle STANDARD_ANGLES
public static final FormboardLayoutBuilder.BranchAngle MAXIMUM_ANGLES
public static final FormboardLayoutBuilder.BranchAngle RANDOM_ANGLES
public static final int _AS_DESIGNED
public static final int _STANDARD_ANGLES
public static final int _MAXIMUM_ANGLES
public static final int _RANDOM_ANGLES
public static FormboardLayoutBuilder.BranchAngle valueOf(int value)
public static FormboardLayoutBuilder.BranchAngle valueOf(String name)
public static FormboardLayoutBuilder.BranchAngle[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.