Package | Description |
---|---|
nxopen.formboard |
Provides interfaces and classes to the Routing Electrical Formboard functionality.
|
Modifier and Type | Field and Description |
---|---|
static UpdateDiscrepancy.Type |
UpdateDiscrepancy.Type.EXTRA
Object is in the formboard but not in
the 3D harness.
|
static UpdateDiscrepancy.Type |
UpdateDiscrepancy.Type.MISSING
Object exits in the 3D harness but is
missing from the formboard.
|
static UpdateDiscrepancy.Type |
UpdateDiscrepancy.Type.MODIFIED
Object exists in both 3D and the formboard but
is modified in some way.
|
static UpdateDiscrepancy.Type |
UpdateDiscrepancy.Type.UNKNOWN
Unknown type, not valid.
|
Modifier and Type | Method and Description |
---|---|
UpdateDiscrepancy.Type |
UpdateDiscrepancy.discrepancyType()
Returns the general type of the discrepancy.
|
static UpdateDiscrepancy.Type |
UpdateDiscrepancy.Type.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static UpdateDiscrepancy.Type |
UpdateDiscrepancy.Type.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static UpdateDiscrepancy.Type[] |
UpdateDiscrepancy.Type.values()
Returns an array that contains the values for this enum.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.