Package | Description |
---|---|
nxopen.formboard |
Provides interfaces and classes to the Routing Electrical Formboard functionality.
|
Modifier and Type | Field and Description |
---|---|
static ObjectAttributeReferenceBuilder.LeaderType |
ObjectAttributeReferenceBuilder.LeaderType.NONE
No leader for annotation of selected object.
|
static ObjectAttributeReferenceBuilder.LeaderType |
ObjectAttributeReferenceBuilder.LeaderType.SINGLE_LOCATION
Single leader for the annotation of selected object.
|
static ObjectAttributeReferenceBuilder.LeaderType |
ObjectAttributeReferenceBuilder.LeaderType.STARTAND_END_LOCATIONS
Two leaders for annotation with start and end location.
|
Modifier and Type | Method and Description |
---|---|
ObjectAttributeReferenceBuilder.LeaderType |
ObjectAttributeReferenceBuilder.enumType()
Returns the enum type
License requirements: routing_harness ("Routing Harness") . |
static ObjectAttributeReferenceBuilder.LeaderType |
ObjectAttributeReferenceBuilder.LeaderType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ObjectAttributeReferenceBuilder.LeaderType |
ObjectAttributeReferenceBuilder.LeaderType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ObjectAttributeReferenceBuilder.LeaderType[] |
ObjectAttributeReferenceBuilder.LeaderType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ObjectAttributeReferenceBuilder.setEnumType(ObjectAttributeReferenceBuilder.LeaderType enumType)
License requirements: routing_harness ("Routing Harness") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.