Interface | Description |
---|---|
AddFontBuilder |
Builder for creating an add font user interface dialogue
To obtain an instance of this class use AddFontBuilder Created in NX8.5.0 |
Anchor |
A Routing Anchor defines a position in a Qualified Routing component part.
|
AnchorCollection |
Represents a collection of
Anchor objects. |
ArcSegment |
Represents a arc segment.
|
ArcSegmentCollection |
Represents a collection of
ArcSegment objects. |
AssemblyDefinition |
Represents a collection of
SingleDevice objects that are used in an assembled product. |
AssignCornerBuilder |
Builder class for Assign Corner which creates corner
To create a new instance of this class, use RouteManager.createAssignCornerBuilder() Default values. |
AssignDiscontinuityBuilder |
the Builder to Assign Discontinuity for the stocks
To create a new instance of this class, use RouteManager.createAssignDiscontinuityBuilder(nxopen.NXObject) Created in NX7.5.0 |
AssignPathBuilder |
Assigns path to a broken routing run
To create a new instance of this class, use RouteManager.createAssignPathBuilder(nxopen.routing.Run) Created in NX8.5.0 |
AttributeHolder |
Represents a
AttributeHolder
Use Routing.RouteManager#createAttributeHolder to get the instance of this class. |
AttributeMembersBuilder |
Creates attibutemembers builder object to add to the search criteria list used by FindByAttributesBuilder
To create a new instance of this class, use FindByAttributesBuilder.attributeMembersBuilder() Created in NX8.5.0 |
BendCorner |
Computes a fillet curve between two linear segments to form a smooth
bend transition from one segment to another.
|
BendCornerCollection |
Represents a collection of
BendCorner objects. |
BranchPathNumberingBuilder |
Builder class for Branch Path Numbering.
|
BuiltInPath |
The Routing BuiltInPath object stores a set of curves.
|
BuiltInPathCollection |
Represents a collection of
BuiltInPath objects. |
CharacteristicList |
Contains a list of characteristics.
|
ClockPartBuilder |
Builder class for clock part object
To create a new instance of this class, use RouteManager.createClockPartBuilder(nxopen.NXObject) Default values. |
CompareRunsBuilder |
Represents a
CompareRunsBuilder , used to compare runs in the work
part to the ones in another part, or to runs defined in xml files gathered in a folder
(native mode) or on an item revision (managed mode). |
ConnectedCurvesBuilder |
Builder for creating automatically creating segments on end-to-end connected
curves.
|
ConnectivityDefinition |
The base class for various connection objects.
|
ConnectPathBuilder |
Represents a
ConnectPathBuilder . |
ControlPoint |
Routing Control Points define a position in space, and are used to determine connections
from segments to segments, and segments to ports.
|
ControlPointCollection |
Represents a collection of
ControlPoint objects. |
CopeCorner |
The cope corner is a corner that trims stocks at a junction.
|
CopeCornerBuilder | Deprecated
Deprecated in NX8.0.0.
|
CopeCornerCollection |
Represents a collection of
CopeCorner objects. |
Corner |
The Routing Corner is the abstract parent class of all other corner objects.
|
CornerCollection |
Represents a collection of
Corner objects. |
CornerTypeBuilder |
Contains setting for corner creation.
|
CreateFabricationBuilder |
Builder class to fabricate subassembly from standard parts, path segments, stock, and other routing objects within the current routing assembly
To create a new instance of this class, use RouteManager.createFabricationBuilder(nxopen.NXObject[]) Created in NX8.0.0 |
CrossSection |
A
CrossSection defines a profile to sweep for Stock objects. |
CrossSectionCollection |
Represents a collection of
CrossSection objects. |
DefineRunBuilder |
Builder Class for DefineRun Object
To create a new instance of this class, use RouteManager.createDefineRunBuilder(nxopen.routing.Run) Created in NX8.5.0 |
DeleteFontsBuilder |
Represents a
DeleteFontsBuilder
To create a new instance of this class, use RouteManager.createDeleteFontsBuilder(nxopen.NXObject[]) Created in NX8.5.0 |
DeleteGapsBuilder |
Represents a
DeleteGapsBuilder
To create a new instance of this class, use RouteManager.createDeleteGapsBuilder(nxopen.NXObject[]) Created in NX8.5.0 |
DeleteObjectsBuilder |
Represents a
DeleteObjectsBuilder
To create a new instance of this class, use RouteManager.createDeleteObjectsBuilder(nxopen.NXObject[]) Created in NX6.0.0 |
DesignRule |
Represents
DesignRule object Creator not available in KF. |
DesignRuleCollection |
Represents a collection of
DesignRule objects. |
DesignRuleManager |
Represents
DesignRuleManager object Creator not available in KF. |
DesignRuleOverride |
Represents Routing DesignRuleOverride object
Creator not available in KF. |
DesignRuleViolation |
Represents
DesignRuleViolation object Design Rule Violation object is created automatically during design rule check Created in NX4.0.2 |
DesignRuleViolationCollection |
Represents a collection of
DesignRuleViolation objects. |
DesignRuleViolationLocation |
Represents
DesignRuleViolationLocation object Design Rule Violation Location object get created automatically during design rule check Created in NX6.0.0 |
DesignRuleViolationLocationCollection |
Represents a collection of
DesignRuleViolationLocation objects. |
DesignRuleViolationViewer |
This class can be used to set the violation id, update text for overridding the violation and
update the user name used to override the violation.
|
DeviceRelationship |
Represents a relationship between
SingleDevice objects. |
DiscontinuityCorner |
A discontinuity corner is a corner that forces
Routing.Stock objects
to split as they cover the segments attached to the discontinuity corner. |
DiscontinuityCornerCollection |
Represents a collection of
DiscontinuityCorner objects. |
Division |
Represents
Division Creator not available in KF because transient objects are not supported. |
DivisionsBuilder |
Represents a
DivisionsBuilder
Builder for creating/editing splits at an end of a duct. |
DuctReinforcement |
Represents a Duct Reinforcement feature used for creating/editing reinforcements
on the inside or outside of rectangular HVAC ducts.
|
DuctReinforcementBuilder |
Builder for creating/editing duct reinforcements.
|
DuctSizeCalculatorBuilder |
Builder to perform calculations of the duct which is to be used in the HVAC applications.
|
EditBendAngleBuilder |
To create a new instance of this class, use RouteManager.createEditBendAngleBuilder(nxopen.NXObject) Created in NX7.5.0 |
EditCharacteristicsBuilder |
Builder to edit required and optional characteristics of
Routing.Stock
or Assemblies.Component as defined in the application view file. |
EditLineSegmentBuilder |
Builder for the "Edit Line Segment" operation.
|
EditPlacePartBuilder |
To create a new instance of this class, use RouteManager.createEditPlacePartBuilder(nxopen.assemblies.Component) Created in NX10.0.0 |
ElbowSnapSettings |
Helper object used the by
LinearPathBuilder builder. |
Filler |
Represents a Filler .
|
FillerCollection |
Represents a collection of
Stock objects. |
FillerStockBuilder |
Creates Filler stock on selected Segments.
|
FindByAttributesBuilder |
Find runs/objects with specified attribute name and attribute value criteria,
highlight the corresponding nodes in the run navigator and the graphics area
To create a new instance of this class, use RouteManager.createFindByAttributesBuilder() Created in NX8.5.0 |
FittingOverstock |
The
FittingOverstock object represents overstock
applied over the faces of the routing parts. |
FittingOverstockBuilder |
Builder for creating or editing
FittingOverstock objects. |
FittingOverstockCollection |
Represents a collection of
FittingOverstock objects. |
FormboardFrame |
The
FormboardFrame is a (not pure) virtual class. |
FormboardFrameCGM |
Represents a Formboard Frame CGM.
|
FormboardFrameCollection |
Represents a collection of
FormboardFrame objects. |
FormboardFramePattern |
Represents a Formboard Frame Pattern.
|
FormboardFrameRectangle |
Represents a Formboard Frame Rectangle.
|
GapArcSegment |
Represents a gap arc segment.
|
GapDisplayBuilder |
Builder for creating a gap arc object on a line segment.
|
HandrailBuilder |
Represents a
HandrailBuilder
Creates a handrail from a selected point. |
HealPath |
Represents a
HealPath object which holds the data used in the creation of the heal path spline. |
ICharacteristic |
Interface for querying and setting characteristic (UG attribute values) on various
routing objects.
|
InfoObjectsBuilder |
Represents a
InfoObjectsBuilder
To create a new instance of this class, use RouteManager.createInfoObjectsBuilder(nxopen.NXObject[]) Created in NX6.0.0 |
InstanceNameLookupBuilder |
Represents a
InstanceNameLookupBuilder . |
IntegrateRunsBuilder |
Builder Class for Integrate Runs Object
To create a new instance of this class, use RouteManager.integrateRunsBuilder(nxopen.routing.Run, nxopen.routing.Run) Default values. |
InterfaceTerminalBase |
The
InterfaceTerminalBase corresponds to an abstract class for
a prototype nxopen.routing.Port . |
InterfaceTerminalRelationshipBase |
The abstract class
InterfaceTerminalRelationshipBase relates many
nxopen.routing.Port s to one nxopen.routing.Port . |
InterfaceTerminalRelationshipCollection |
Represents a collection of
InterfaceTerminalRelationshipShadow objects. |
InterfaceTerminalRelationshipShadow |
Represents an assembly shadow of
InterfaceTerminalRelationshipBase . |
InterfaceTerminalShadow |
Represents the defining data for a physical
nxopen.routing.Port . |
IPath |
The Routing IPath object is a list of segments in a route.
|
IRoutePosition |
Interface class for all routing objects that specify a single (possibly associative) location
in space.
|
ISegment |
Interface class for all routing segments [Line/Arc/Spline] .
|
ISegmentCollection |
Represents a collection of
Routing.ISegment objects. |
IsoDrawingBuilder |
Represents a
IsoDrawingBuilder , used to run the ISOGEN engine
to create isometric drawings of piping networks. |
ItemDefinition |
ItemDefinition object corresponds to DDID in AP212 and to a piece
part or routing stock in NX. |
LinearPathBuilder |
Builder for creating routing linear paths.
|
LinearPathSettings |
Helper object used the by
Routing.LinearPathBuilder builder. |
LineSegment |
Represents a line segment.
|
LineSegmentCollection |
Represents a collection of
LineSegment objects. |
LogicalTerminal |
Assembly instance of a
InterfaceTerminalBase . |
ManualRouteBuilder |
To create a new instance of this class, use RouteManager.createManualRouteBuilder(nxopen.routing.electrical.ElectricalStockDevice.RouteLevel, nxopen.routing.electrical.ElectricalStockDevice) Created in NX7.5.0 |
MergeStocksBuilder |
Represents a
MergeStocksBuilder
Builder for merging routing stocks ( including space reservation stocks ). |
MiterCorner |
This class defines a mitered corner.
|
MiterCornerCollection |
Represents a collection of
MiterCorner objects. |
MiteredBendCorner |
Computes a fillet curve between two linear segments to form a smooth
bend transition from one segment to another that represents a mitered bend.
|
MiteredBendCornerCollection |
Represents a collection of
MiteredBendCorner objects. |
ModelTerminalsBuilder |
The Builder to Model/UnModel the Terminals
To create a new instance of this class, use RouteManager.modelTerminalsBuilder() Default values. |
ObjectRelationship |
Represents a relationship between Routing objects.
|
OffsetPath |
The Routing OffsetPath object is the set of information needed to define an offset route.
|
OffsetPathCollection |
The Routing OffsetPath object is a list of segments in a route.
|
Overstock |
Represents an
Overstock object. |
OverstockApplication |
Represents a collection of
OverstockApplication objects. |
OverstockApplicationCollection |
Represents a collection of
OverstockApplication objects. |
OverstockBuilder |
Builder for creating/editing overstocks.
|
OverstockFacesBuilder |
Builder for qualifying faces for overstock application over fittings.
|
PartDefinitionBase |
The abstract class
PartDefinitionBase contains
information defining a logical part. |
PartDefinitionShadow |
PartDefinitionShadow contains the defining data for a
logical part, such as an connector. |
Path |
The Routing Path object is the set of ordered continuous segments.
|
PathStockBuilder |
Assigns stocks to segments based of users critiera and the current
default stock.
|
PlacementSolutionsBuilder |
To create a new instance of this class, use RouteManager.createPlacementSolutionsBuilder() Created in NX7.5.0 |
PlacePartBuilder |
To create a new instance of this class, use RouteManager.createPlacePartBuilderPTS(nxopen.TaggedObject, nxopen.TaggedObject, nxopen.Point3d, nxopen.TaggedObject) Created in NX7.5.0 |
Platform | |
PlatformCreatorBuilder |
Builder for creating platform.
|
QuickPathBuilder |
Builder for creating a collision free path between points.
|
RemoveDiscontinuityBuilder |
Builder class for remove discontinuity object
To create a new instance of this class, use RouteManager.createRemoveDiscontinuityBuilder(nxopen.NXObject[]) Created in NX7.5.0 |
ReuseLibrary |
Represents a
ReuseLibrary No creator is available in KF. |
RootObject |
The
RootObject is the parent
class of all other Routing logical objects. |
RouteLogicalAssociation |
RouteLogicalAssociation object associates non-electrical components to
electrical components.
|
RouteLogicalAssociationCollection |
Collection class for RouteLogicalAssociation object
To obtain an instance of this class, refer to RouteManager Created in NX4.0.0 |
RouteManager |
Manages various Routing collections and methods for use in the current work part.
|
RouteObject |
The Top level routing data model object.
|
RouteObjectCollector |
Represents a
RouteObjectCollector class
to create objects for getting routing objects. |
RoutePartDescriptor |
Represents a part descriptor chrx.
|
RoutePartDescriptorCollection |
Represents a collection of
RoutePartDescriptor objects. |
RouteSegmentFont |
Represents a route segment font.
|
RouteSegmentFontElement |
Represents a route segment font element.
|
RouteSweptFoldBuilder |
Represents a Rout Swept Fold Builder
To create a new instance of this class, use RouteManager.createRouteSweptFoldBuilder(nxopen.NXObject, nxopen.NXObject) Created in NX7.0.0 |
RouteSweptTwistBuilder |
To create a new instance of this class, use RouteManager.createRouteSweptTwistBuilder(nxopen.NXObject) Created in NX6.0.0 |
RoutingMeasureDistanceBuilder |
Represents a
RoutingMeasureDistanceBuilder Creator not available in KF because transient objects are not supported. |
RoutingSystem |
Routing object is a collection of
Run objects. |
RoutingSystemCollection |
Represents a collection of
RoutingSystem objects. |
Run |
Routing Run object references components and stocks which comprise a piping run.
|
RunCollection |
Represents a collection of
Run objects. |
RunItem |
Routing Run Item object references components which comprise a piping run.
|
RunItemsBuilder |
The builder for creating the list item of RunItems
To create a new instance of this class, use DefineRunBuilder.createRunItemsBuilder() Created in NX8.5.0 |
RunItemsBuilderList |
Represents a list of objects.
|
SBendCorner |
The Routing SBendCorner defines a S-Bend.
|
SBendCornerCollection |
Represents a collection of
SBendCorner objects. |
SegmentManager |
Contains the type of the routing part as well as the Collection objects for creating/iterating
over routing objects.
|
SegmentPairBuilder |
The builder for creating the list item of SegmentPairs
To create a new instance of this class, use AssignDiscontinuityBuilder.segmentPairBuilder() Created in NX7.5.0 |
SelectControlPoint |
Represents a single object selection.
|
SelectISegment |
Represents a single object selection.
|
SelectLineSegment |
Represents a single object selection.
|
SelectRun |
Represents a single object selection.
|
SelectStock |
Represents a single object selection.
|
SimplifyPathBuilder |
Represents a
SimplifyPathBuilder for Simplify Path operation. |
SingleDevice |
The Routing SingleDevice corresponds to an abstract instance of
ItemDefinition . |
SpaceReservationBuilder |
Represents a
SpaceReservationBuilder
This builder takes one or more segments and creates space reservation stock on it. |
SplinePathBuilder |
Builder for creating a D-Cubed constrained spline.
|
SplineSegment |
Represents a spline segment.
|
SplineSegmentCollection |
Represents a collection of
SplineSegment objects. |
SplitDuctBuilder |
Represents a
SplitDuctBuilder
Builder for creating/editing splits at an end of a duct. |
SplitRunBuilder |
Builder Class for Split Run Object
To create a new instance of this class, use RouteManager.splitRunBuilder(nxopen.routing.Run) Default values. |
Stock |
The
Stock object represents a material (such as as pipe or tube)
that covers a path of segments. |
StockBrowserBuilder |
Builder class for stock browser .
|
StockBuilder |
Builder for creating/editing stocks.
|
StockCollection |
Represents a collection of
Stock objects. |
StockColorBuilder |
Represents a
StockColorBuilder . |
StockData | |
StockDataCollection |
Represents a collection of
StockData objects. |
StockDefinition |
Represents Routing StockDefinition object
Creator not available in KF. |
StockDevice |
The Routing StockDevice corresponds to a generic stock instance
of
Routing.SingleDevice . |
StockOffsetPointBuilder |
Applies Assemblies Constraints to a selected
Point or
ControlPoint to mimic the update/move behavior of
the input smart Point . |
StockPartConverterBuilder |
Represents a
StockPartConverterBuilder
Builder for Part Conversion of the stocks. |
StockStyleBuilder |
Builder class to assigns style to the selected stock .
|
StockTransition |
Represents
StockTransition object. |
StockTransitionBuilder |
Builder for creating/editing stockTransition.
|
SubdivideSegmentBuilder |
Represents a
SubdivideSegmentBuilder . |
TransformPathBuilder |
Builder for the "Transform Path" operation.
|
UnifyPathBuilder |
Builder to unify
Routing.Stock and Assemblies.Component
based on specified characteristic values. |
WatertightFittingsBuilder |
Represents a
WatertightFittingsBuilder To create a new instance of this class, use RouteManager.createWatertightFittingsBuilder() Created in NX8.0.0 |
WindCatcher |
Represents a Wind Catcher feature.
|
WindCatcherBuilder |
Builder class for Wind Catcher feature.
|
Wire |
The Routing Wire object is the set of information needed to define
a ROUTE_wire.
|
WireCollection |
The Routing Wire object is a list of segments in a route and some
stock.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.