Package | Description |
---|---|
nxopen.formboard |
Provides interfaces and classes to the Routing Electrical Formboard functionality.
|
Modifier and Type | Field and Description |
---|---|
static LayoutLengthOptions.RoundingMethod |
LayoutLengthOptions.RoundingMethod.DOWN_TO_NEAREST
Lengths are rounded down to
the nearest increment value.
|
static LayoutLengthOptions.RoundingMethod |
LayoutLengthOptions.RoundingMethod.EXACT
Lengths are unmodified.
|
static LayoutLengthOptions.RoundingMethod |
LayoutLengthOptions.RoundingMethod.NEAREST
Lengths are rounded up or down
to the nearest increment value.
|
static LayoutLengthOptions.RoundingMethod |
LayoutLengthOptions.RoundingMethod.UP_TO_NEAREST
Lengths are rounded up to the
nearest increment value.
|
Modifier and Type | Method and Description |
---|---|
LayoutLengthOptions.RoundingMethod |
LayoutLengthOptions.netlistRoundingMethod()
Returns the rounding method to apply to Connection List lengths.
|
LayoutLengthOptions.RoundingMethod |
LayoutLengthOptions.overstockRoundingMethod()
Returns the rounding method to apply to overstock wrapped lengths.
|
LayoutLengthOptions.RoundingMethod |
LayoutLengthOptions.segmentRoundingMethod()
Returns the rounding method to apply to segment lengths.
|
static LayoutLengthOptions.RoundingMethod |
LayoutLengthOptions.RoundingMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LayoutLengthOptions.RoundingMethod |
LayoutLengthOptions.RoundingMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LayoutLengthOptions.RoundingMethod[] |
LayoutLengthOptions.RoundingMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LayoutLengthOptions.setNetlistRoundingMethod(LayoutLengthOptions.RoundingMethod netlistRoundingMethod)
License requirements: routing_harness ("Routing Harness") . |
void |
LayoutLengthOptions.setOverstockRoundingMethod(LayoutLengthOptions.RoundingMethod overstockRoundingMethod)
License requirements: routing_harness ("Routing Harness") . |
void |
LayoutLengthOptions.setSegmentRoundingMethod(LayoutLengthOptions.RoundingMethod segmentRoundingMethod)
License requirements: routing_harness ("Routing Harness") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.