Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.cae.modelcheck |
Provides classes and interfaces for Model Check.
|
Class and Description |
---|
AlignShellElementNormalBuilder
Represents a
AlignShellElementNormalBuilder builder used to align the normals of
connected shell elements with a seed shell element. |
DuplicateElementsCheckBuilder
Represents a
DuplicateElementsCheckBuilder
to check for duplicate elements within the candidate elements. |
DuplicateNodesCheckBuilder
Represents a
DuplicateNodesCheckBuilder
to check for duplicate nodes within the candidate nodes. |
ElementEdgeCheckBuilder
Represents a
ElementEdgeCheckBuilder which can be
used to detect free element edges or non-manifold edges. |
ElementMaterialOrientationCheckBuilder
Represents a
ElementMaterialOrientationCheckBuilder
used to check the material orientation for shell and solid elements. |
ElementQualityCheckBuilder
Represents a
ElementQualityCheckBuilder to
perform quality checking on the candidate elements. |
ElementQualitySettingCollection
Represents a collection of
ElementQualitySetting in a cae part. |
FaceClearanceCheckBuilder
Represents a
FaceClearanceCheckBuilder to perform polygon face
interference or clearance check. |
ModelSetupCheckBuilder
Represents a
ModelSetupCheckBuilder which can be
used to check if the active SimSolution contains all the necessary
items for the analysis, including elements, loads, constraints and materials. |
ReverseShellElementNormalBuilder
Represents a
ReverseShellElementNormalBuilder used to reverse normals
for specified shell elements. |
Class and Description |
---|
AlignShellElementNormalBuilder.ConnectedElementScope
the options to define the connection scope to the seed element for model checking
|
DuplicateElementsCheckBuilder.DeletePreference
Represents the duplicate elements deleting preference
|
DuplicateElementsCheckBuilder.DisplaySettings
Represents the display settings of duplicated elements detected
|
DuplicateNodesCheckBuilder.DisplaySettings
Represents the display settings data
|
DuplicateNodesCheckBuilder.ListOption
Represents the duplicate nodes merging preference
|
DuplicateNodesCheckBuilder.MergePreference
Represents the duplicate nodes merging preference
|
ElementEdgeCheckBuilder.EdgeDisplayStyle
the display style of the edges detected
|
ElementEdgeCheckBuilder.ExecuteCheckData
This class holds the data returned from
ElementEdgeCheckBuilder.executeCheck() |
ElementEdgeCheckBuilder.Scope
the Scope over which the Computation of free/non-manifold edges with be done
|
ElementMaterialOrientationCheckBuilder.DoCheckData
This class holds the data returned from
ElementMaterialOrientationCheckBuilder.doCheck() |
ElementMaterialOrientationCheckBuilder.MaterialOrientationType
the material orientation type
|
ElementQualityCheckBuilder.OutputElements
indicates how to create output group
|
ElementQualityCheckBuilder.ReportFormat
indicates how to generate report
|
ElementQualityCheckResults
Represents the element quality checking result of
ElementQualityCheckBuilder
To obtain an instance of this class use CAE.ModelCheck.ElementQualityCheckBuilder Created in NX8.5.0 |
ElementQualityCheckResults.TestSummary
Reprents the summary data of a specified quality checking test type
|
ElementQualitySetting
Represents element quality check settings of a specified solver language.
|
ElementQualitySetting.LimitValue
indicates how criteria value is defined
|
ElementSpecificTestValue
Represents the quality setting for a specfied element reference
Not to support KF . |
ElementTestResult
Represents quality checking result for an element.
|
ITestValue
Represents the quality check criteria value settings
This is an abstract class, and cannot be instantiated. |
ITestValue.CriteriaValueData
This class holds the data returned from
ITestValue.getCriteriaValue(nxopen.cae.modelcheck.TestValueTypes.CriteriaType) |
ITestValue.IsSolverSpecificTestData
This class holds the data returned from
ITestValue.getIsSolverSpecificTest() |
QualityTestValue
Represents quality test settings of a specified test type
Not to support KF . |
TestResult
Represents quality checking result of a quality test
To obtain an instance of this class use CAE.ModelCheck.ElementTestResult.GetTestResults Created in NX8.5.0 |
TestValueTypes.CriteriaType
the alert level of a criteria value
|
TestValueTypes.ElementReference
represents an element reference definition associated with this test
|
TestValueTypes.Result
the checking result
|
TestValueTypes.TestType
the test types
|
TestValueTypes.Validator
indicates how to compare the check result with the criteria value
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.