Package | Description |
---|---|
nxopen.cae.modelcheck |
Provides classes and interfaces for Model Check.
|
Modifier and Type | Field and Description |
---|---|
ElementMaterialOrientationCheckBuilder.MaterialOrientationType[] |
ElementMaterialOrientationCheckBuilder.DoCheckData.orientationtype |
static ElementMaterialOrientationCheckBuilder.MaterialOrientationType |
ElementMaterialOrientationCheckBuilder.MaterialOrientationType.SHELL
the material orientation of shell element
|
static ElementMaterialOrientationCheckBuilder.MaterialOrientationType |
ElementMaterialOrientationCheckBuilder.MaterialOrientationType.SOLID_FIRST_DIRECTION
the first direction of solid element material orientation
|
static ElementMaterialOrientationCheckBuilder.MaterialOrientationType |
ElementMaterialOrientationCheckBuilder.MaterialOrientationType.SOLID_SECOND_DIRECTION
the second direction of solid element material orientation
|
static ElementMaterialOrientationCheckBuilder.MaterialOrientationType |
ElementMaterialOrientationCheckBuilder.MaterialOrientationType.SOLID_THIRD_DIRECTION
the third direction of solid element material orientation
|
Modifier and Type | Method and Description |
---|---|
static ElementMaterialOrientationCheckBuilder.MaterialOrientationType |
ElementMaterialOrientationCheckBuilder.MaterialOrientationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ElementMaterialOrientationCheckBuilder.MaterialOrientationType |
ElementMaterialOrientationCheckBuilder.MaterialOrientationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ElementMaterialOrientationCheckBuilder.MaterialOrientationType[] |
ElementMaterialOrientationCheckBuilder.MaterialOrientationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
boolean |
ElementMaterialOrientationCheckBuilder.getCheckOrientation(ElementMaterialOrientationCheckBuilder.MaterialOrientationType orientationType)
Gets option value which indicates whether to check for the specified material orientation type
License requirements: None. |
NXColor |
ElementMaterialOrientationCheckBuilder.getOrientationColor(ElementMaterialOrientationCheckBuilder.MaterialOrientationType orientationType)
Gets display color of a specified material orientation type
License requirements: None. |
void |
ElementMaterialOrientationCheckBuilder.setCheckOrientation(ElementMaterialOrientationCheckBuilder.MaterialOrientationType orientationType,
boolean checkOrientation)
Sets option value which indicates whether to check for the specified material orientation type
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
ElementMaterialOrientationCheckBuilder.setOrientationColor(ElementMaterialOrientationCheckBuilder.MaterialOrientationType orientationType,
NXColor color)
Sets display color of a specified material orientation type
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.