Package | Description |
---|---|
nxopen.cae.modelcheck |
Provides classes and interfaces for Model Check.
|
Modifier and Type | Field and Description |
---|---|
static ElementQualitySetting.LimitValue |
ElementQualitySetting.LimitValue.ERROR_LIMIT_ONLY
Only error criteria value could be defined
|
static ElementQualitySetting.LimitValue |
ElementQualitySetting.LimitValue.WARNING_AND_ERROR_LIMIT
Both warning and error criteria value could be defined
|
Modifier and Type | Method and Description |
---|---|
ElementQualitySetting.LimitValue |
ElementQualitySetting.limitValueOption()
Returns the limit value option
License requirements: None. |
static ElementQualitySetting.LimitValue |
ElementQualitySetting.LimitValue.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ElementQualitySetting.LimitValue |
ElementQualitySetting.LimitValue.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ElementQualitySetting.LimitValue[] |
ElementQualitySetting.LimitValue.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ElementQualitySetting.setLimitValueOption(ElementQualitySetting.LimitValue limitValueOption)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.