public interface ReverseShellElementNormalBuilder extends Builder
ReverseShellElementNormalBuilder
used to reverse normals
for specified shell elements. You can reverse shell element normals by using either Builder.commit()
or reverseNormals()
.
The difference between these two methods is Builder.commit()
reverses the normals
and updates normal display, but it does not return the shell elements which were reversed
successfully. reverseNormals()
reverses normals and returns the shell elements which were reversed successfully.
Both of the methods are only available in fem context.
nxopen.cae.modelcheckManager#createReverseShellElementNormalBuilder
Modifier and Type | Method and Description |
---|---|
void |
displayNormals()
Display normals of
selectionList()
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX8.5.0 |
FEElement[] |
reverseNormals()
Reverses normals specified in
selectionList()
and returns those elements whose normals were reversed successfully. |
SelectTaggedObjectList |
selectionList()
Returns the selected objects to be checked.
|
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
SelectTaggedObjectList selectionList() throws NXException, RemoteException
Mesh
or
FEElement
NXException
RemoteException
void displayNormals() throws NXException, RemoteException
selectionList()
NXException
RemoteException
FEElement[] reverseNormals() throws NXException, RemoteException
selectionList()
and returns those elements whose normals were reversed successfully. This method will only reverse
the normals for shell elements in the current work fem part.
NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.