Package | Description |
---|---|
nxopen.cae.modelcheck |
Provides classes and interfaces for Model Check.
|
Modifier and Type | Field and Description |
---|---|
static TestValueTypes.TestType |
TestValueTypes.TestType.ASPECT_RATIO |
static TestValueTypes.TestType |
TestValueTypes.TestType.AXISYMMETRIC_X
When elements are modeled in XZ plane,
check X >= 0.0.
|
static TestValueTypes.TestType |
TestValueTypes.TestType.AXISYMMETRIC_Y
When elements are modeled in XZ plane,
check consistent Y.
|
static TestValueTypes.TestType |
TestValueTypes.TestType.COHESIVE_ELEMENT |
static TestValueTypes.TestType |
TestValueTypes.TestType.EDGE_POINT_INCLUDED_ANGLE |
static TestValueTypes.TestType |
TestValueTypes.TestType.EDGE_POINT_LENGTH_RATIO |
static TestValueTypes.TestType |
TestValueTypes.TestType.FACE_WARP_COEFFICIENT |
static TestValueTypes.TestType |
TestValueTypes.TestType.INTERIOR_ANGLE_MAXIMUM |
static TestValueTypes.TestType |
TestValueTypes.TestType.INTERIOR_ANGLE_MINIMUM |
static TestValueTypes.TestType |
TestValueTypes.TestType.JACOBIAN_RATIO |
static TestValueTypes.TestType |
TestValueTypes.TestType.JACOBIAN_SIGN |
static TestValueTypes.TestType |
TestValueTypes.TestType.JACOBIAN_ZERO |
static TestValueTypes.TestType |
TestValueTypes.TestType.LENGTH_MAXIMUM |
static TestValueTypes.TestType |
TestValueTypes.TestType.LENGTH_MINIMUM |
static TestValueTypes.TestType |
TestValueTypes.TestType.LENGTH_RATIO_OFFSET |
static TestValueTypes.TestType |
TestValueTypes.TestType.PARALLEL_DEVIATION |
static TestValueTypes.TestType |
TestValueTypes.TestType.SHAPE_FACTOR |
static TestValueTypes.TestType |
TestValueTypes.TestType.SKEW_ANGLE |
static TestValueTypes.TestType |
TestValueTypes.TestType.TAPER |
TestValueTypes.TestType |
ElementQualityCheckResults.TestSummary.testType
the test type
|
static TestValueTypes.TestType |
TestValueTypes.TestType.TET_COLLAPSE |
static TestValueTypes.TestType |
TestValueTypes.TestType.TWIST |
static TestValueTypes.TestType |
TestValueTypes.TestType.VOLUME |
static TestValueTypes.TestType |
TestValueTypes.TestType.WARP_FACTOR |
static TestValueTypes.TestType |
TestValueTypes.TestType.WARPAGE_ANGLE |
Modifier and Type | Method and Description |
---|---|
TestValueTypes.TestType |
ITestValue.getTestType()
Returns the test type
License requirements: None. |
TestValueTypes.TestType |
TestResult.testType()
Returns the test type
License requirements: None. |
static TestValueTypes.TestType |
TestValueTypes.TestType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TestValueTypes.TestType |
TestValueTypes.TestType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TestValueTypes.TestType[] |
TestValueTypes.TestType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
QualityTestValue |
ElementQualitySetting.getTestValueByType(TestValueTypes.TestType testType)
|
String |
ElementQualitySetting.locateTestDescriptorName(FEElement element,
TestValueTypes.TestType testType,
boolean useElemSpecific)
Returns the name of a quality test value, which is associated with
an element for a specified test type
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Constructor and Description |
---|
TestSummary(TestValueTypes.TestType testTypeInitial,
double worstTestValueInitial,
boolean hasTestValueInitial,
int testCountInitial,
int errorCountInitial,
int warnedCountInitial)
Constructor for the TestSummary object.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.