public static class TestValueTypes.TestType extends Enum
Modifier and Type | Method and Description |
---|---|
static TestValueTypes.TestType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TestValueTypes.TestType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TestValueTypes.TestType[] |
values()
Returns an array that contains the values for this enum.
|
public static final TestValueTypes.TestType JACOBIAN_ZERO
public static final TestValueTypes.TestType JACOBIAN_RATIO
public static final TestValueTypes.TestType JACOBIAN_SIGN
public static final TestValueTypes.TestType VOLUME
public static final TestValueTypes.TestType AXISYMMETRIC_Y
public static final TestValueTypes.TestType AXISYMMETRIC_X
public static final TestValueTypes.TestType ASPECT_RATIO
public static final TestValueTypes.TestType SKEW_ANGLE
public static final TestValueTypes.TestType INTERIOR_ANGLE_MINIMUM
public static final TestValueTypes.TestType INTERIOR_ANGLE_MAXIMUM
public static final TestValueTypes.TestType TAPER
public static final TestValueTypes.TestType WARP_FACTOR
public static final TestValueTypes.TestType FACE_WARP_COEFFICIENT
public static final TestValueTypes.TestType EDGE_POINT_LENGTH_RATIO
public static final TestValueTypes.TestType EDGE_POINT_INCLUDED_ANGLE
public static final TestValueTypes.TestType LENGTH_RATIO_OFFSET
public static final TestValueTypes.TestType PARALLEL_DEVIATION
public static final TestValueTypes.TestType SHAPE_FACTOR
public static final TestValueTypes.TestType TWIST
public static final TestValueTypes.TestType LENGTH_MINIMUM
public static final TestValueTypes.TestType LENGTH_MAXIMUM
public static final TestValueTypes.TestType TET_COLLAPSE
public static final TestValueTypes.TestType WARPAGE_ANGLE
public static final TestValueTypes.TestType COHESIVE_ELEMENT
public static final int _JACOBIAN_ZERO
public static final int _JACOBIAN_RATIO
public static final int _JACOBIAN_SIGN
public static final int _VOLUME
public static final int _AXISYMMETRIC_Y
public static final int _AXISYMMETRIC_X
public static final int _ASPECT_RATIO
public static final int _SKEW_ANGLE
public static final int _INTERIOR_ANGLE_MINIMUM
public static final int _INTERIOR_ANGLE_MAXIMUM
public static final int _TAPER
public static final int _WARP_FACTOR
public static final int _FACE_WARP_COEFFICIENT
public static final int _EDGE_POINT_LENGTH_RATIO
public static final int _EDGE_POINT_INCLUDED_ANGLE
public static final int _LENGTH_RATIO_OFFSET
public static final int _PARALLEL_DEVIATION
public static final int _SHAPE_FACTOR
public static final int _TWIST
public static final int _LENGTH_MINIMUM
public static final int _LENGTH_MAXIMUM
public static final int _TET_COLLAPSE
public static final int _WARPAGE_ANGLE
public static final int _COHESIVE_ELEMENT
public static TestValueTypes.TestType valueOf(int value)
public static TestValueTypes.TestType valueOf(String name)
public static TestValueTypes.TestType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.