Package | Description |
---|---|
nxopen.cae.modelcheck |
Provides classes and interfaces for Model Check.
|
Modifier and Type | Field and Description |
---|---|
static AlignShellElementNormalBuilder.ConnectedElementScope |
AlignShellElementNormalBuilder.ConnectedElementScope.ALL_VISIBLE
Limits check to only those shell elements which are connected to the Seed Element and are currently visible
|
static AlignShellElementNormalBuilder.ConnectedElementScope |
AlignShellElementNormalBuilder.ConnectedElementScope.SEED_MESH
Limits check to only those shell elements in the mesh that contains the Seed Element
|
static AlignShellElementNormalBuilder.ConnectedElementScope |
AlignShellElementNormalBuilder.ConnectedElementScope.USER_SPECIFIED
Limits check to only those shell elements specified in
AlignShellElementNormalBuilder.userSpecifiedConnectElements() |
Modifier and Type | Method and Description |
---|---|
AlignShellElementNormalBuilder.ConnectedElementScope |
AlignShellElementNormalBuilder.elementConnectScope()
Returns the option to indicate how to define connected elements for checking
License requirements: None. |
static AlignShellElementNormalBuilder.ConnectedElementScope |
AlignShellElementNormalBuilder.ConnectedElementScope.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AlignShellElementNormalBuilder.ConnectedElementScope |
AlignShellElementNormalBuilder.ConnectedElementScope.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AlignShellElementNormalBuilder.ConnectedElementScope[] |
AlignShellElementNormalBuilder.ConnectedElementScope.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AlignShellElementNormalBuilder.setElementConnectScope(AlignShellElementNormalBuilder.ConnectedElementScope connectScope)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.