NXOpen.UserDefinedObjects Package¶
Classes¶
NXOpen.UserDefinedObjects.UserDefinedClass |
JA interface for the UserDefinedClass object |
NXOpen.UserDefinedObjects.UserDefinedClassManager |
JA interface for the UserDefinedClassManager object |
NXOpen.UserDefinedObjects.UserDefinedDisplayEvent |
Implements the Display Event Object for UDO’s |
NXOpen.UserDefinedObjects.UserDefinedEvent |
Implements the Event Object for UDO’s |
NXOpen.UserDefinedObjects.UserDefinedLinkEvent |
Implements the Display Event Object for UDO’s |
NXOpen.UserDefinedObjects.UserDefinedObject |
JA interface for the UserDefinedObject object |
NXOpen.UserDefinedObjects.UserDefinedObjectDisplayContext |
This class is used to display User Defined Objects |
NXOpen.UserDefinedObjects.UserDefinedObjectManager |
This class creates and manages UserDefinedObjects |
Enumerations¶
Structs¶
UserDefinedObjectLinkDefinition_Struct Struct | Contains the linked object and it’s status along with the type of link. |
UserDefinedObjectManagerLinkedUdoDefinition_Struct Struct | Used to define a link to a UserDefinedObject |