UserDefinedEvent Class¶
-
class
NXOpen.UserDefinedObjects.
UserDefinedEvent
¶ Bases:
NXOpen.TransientObject
Implements the Event Object for UDO’s
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
EventReason | Returns the reason we fired this event. |
UserDefinedObject | Returns the related UDO. |
Enumerations¶
UserDefinedEventReason Enumeration | Available link types for a UserDefinedObject . |
Property Detail¶
EventReason¶
-
UserDefinedEvent.
EventReason
¶ Returns the reason we fired this event.
-------------------------------------
Getter Method
Signature
EventReason()
Returns: The reason for the event Return type: NXOpen.UserDefinedObjects.UserDefinedEventReason
New in version NX5.0.0.
License requirements: None.
UserDefinedObject¶
-
UserDefinedEvent.
UserDefinedObject
¶ Returns the related UDO.
-------------------------------------
Getter Method
Signature
UserDefinedObject()
Returns: The UDO that caused the event to fire Return type: NXOpen.UserDefinedObjects.UserDefinedObject
New in version NX5.0.0.
License requirements: None.
Method Detail¶
Dispose¶
-
UserDefinedEvent.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET and Java, his method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX5.0.0.
License requirements: None.