UserDefinedEventReason Enumeration¶
NXOpen.UserDefinedObjects.UserDefinedEvent.Reason is an alias for NXOpen.UserDefinedObjects.UserDefinedEventReason
-
class
NXOpen.UserDefinedObjects.
UserDefinedEventReason
¶ Bases:
object
Available link types for a
UserDefinedObject
.Enum Members
Enum Member Enum Member Description Display Display UDO eventDelete An associated object was deleted - UDO cleanup eventUpdate Update UDO eventSelection Select UDO eventFit Fit display eventAttentionPoint Find Attention Point for the UDO eventInfo Query UDO Information eventEdit Edit UDO eventSuppress Suppress/Unsuppress UDO eventScreenSizeFit Fit operation for screen-size geometry-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-