UserDefinedDisplayEvent Class¶
-
class
NXOpen.UserDefinedObjects.
UserDefinedDisplayEvent
¶ Bases:
NXOpen.UserDefinedObjects.UserDefinedEvent
Implements the Display Event Object for UDO’s
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
DisplayContext | Returns the display context. |
EventReason | Returns the reason we fired this event. |
UserDefinedObject | Returns the related UDO. |
Property Detail¶
DisplayContext¶
-
UserDefinedDisplayEvent.
DisplayContext
¶ Returns the display context.
-------------------------------------
Getter Method
Signature
DisplayContext()
Returns: The context of the given display event Return type: NXOpen.UserDefinedObjects.UserDefinedObjectDisplayContext
New in version NX5.0.0.
License requirements: None.
Method Detail¶
Dispose¶
-
UserDefinedDisplayEvent.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET and Java, his method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX5.0.0.
License requirements: None.