UserDefinedObjectDisplayContextFacetType Enumeration¶
NXOpen.UserDefinedObjects.UserDefinedObjectDisplayContext.FacetType is an alias for NXOpen.UserDefinedObjects.UserDefinedObjectDisplayContextFacetType
-
class
NXOpen.UserDefinedObjects.
UserDefinedObjectDisplayContextFacetType
¶ Bases:
object
The enumerated type facet to be displayed
Enum Members
Enum Member Enum Member Description Triangle The facet topology is a triangle facetPolygon The facet topology is a polygon facetTristrip The facet topology is a tristrip facet-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-