UserDefinedObjectDisplayContextStandardTextRef Enumeration¶
NXOpen.UserDefinedObjects.UserDefinedObjectDisplayContext.StandardTextRef is an alias for NXOpen.UserDefinedObjects.UserDefinedObjectDisplayContextStandardTextRef
-
class
NXOpen.UserDefinedObjects.
UserDefinedObjectDisplayContextStandardTextRef
¶ Bases:
object
This enumerated type specifies the type of reference point used in the text box for standard_text methods.
Enum Members
- default reference point position “
- “BaselineStart”, ” Display the text starting on the
baseline, at the left end of the text box for left-to-right text, or at the right end of the text box for right-to-left text “
“BaselineCenter”, ” Display the text with the given positionin the horizontal center of the text box at the baseline “
“BaselineEnd”, ” Display the text starting on the baseline,at the right end of the text box for left-to-right text, or at the left end of the text box for right-to-left text “
“TopLeft”, ” Display the text with the given position- in the top left of the text box “
- “TopCenter”, ” Display the text with the given position
- in the top center of the text box “
- “TopRight”, ” Display the text with the given position
- in the top right of the text box “
- “MiddleLeft”, ” Display the text with the given position
- in the middle left of the text box “
- “MiddleCenter”, ” Display the text with the given position
- in middle center of text box “
- “MiddleRight”, ” Display the text with the given position
- in middle right of text box “
- “BottomLeft”, ” Display the text with the given position
- in bottom left of text box “
- “BottomCenter”, ” Display the text with the given position
- in bottom center of text box “
- “BottomRight”, ” Display the text with the given position
in bottom right of text box “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.