UserDefinedObjectLinkDefinition_Struct Struct¶
NXOpen.UserDefinedObjects.UserDefinedObject.LinkDefinition is an alias for NXOpen.UserDefinedObjects.UserDefinedObjectLinkDefinition_Struct
-
class
NXOpen.UserDefinedObjects.
UserDefinedObjectLinkDefinition_Struct
¶ Bases:
object
Contains the linked object and it’s status along with the type of link.
Fields¶
Field | Description |
---|---|
AssociatedObject | linked object |
Status | status of the linked object |
AssociatedObject¶
-
UserDefinedObjectLinkDefinition_Struct.
AssociatedObject
¶ linked object
-------------------------------------
Getter Method Signature
AssociatedObject()
Returns: Return type: NXOpen.TaggedObject
-------------------------------------
Setter Method
Signature
AssociatedObject(value)
Parameters: value ( NXOpen.TaggedObject
) –
Status¶
-
UserDefinedObjectLinkDefinition_Struct.
Status
¶ status of the linked object
-------------------------------------
Getter Method Signature
Status()
Returns: Return type: NXOpen.UserDefinedObjects.UserDefinedObjectLinkStatus
-------------------------------------
Setter Method
Signature
Status(value)
Parameters: value ( NXOpen.UserDefinedObjects.UserDefinedObjectLinkStatus
) –