Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
nxopen.mechatronics |
Provides classes and interfaces for Mechatronics.
|
nxopen.routing |
Provides classes and interfaces for Routing.
|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Method and Description |
---|---|
SelectFaceList |
SurfaceUVDirectionBuilder.targetFace()
Returns the target face; feature faces can not be operated on.
|
Modifier and Type | Method and Description |
---|---|
SelectFaceList |
SurfaceRegions.boundaryFaces()
Returns the boundary faces
License requirements: None. |
SelectFaceList |
SurfaceRegions.excludedFaces()
Returns the excluded faces
License requirements: None. |
SelectFaceList |
SurfaceRegions.faces()
Returns the faces
License requirements: None. |
SelectFaceList |
NCAssistantBuilder.facesToAnalyze()
Returns the Faces to Analyze
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
SelectFaceList |
SvtBuilder.backgroundFaces()
Returns the background faces that are to be shown in the section view.
|
Modifier and Type | Method and Description |
---|---|
SelectFaceList |
LatticeBuilder.baseFace()
Returns the faces that the user selects to define the boundary
License requirements: None. |
SelectFaceList |
ExtractFaceBuilder.boundaryFaces()
Returns the boundary faces
License requirements: None. |
SelectFaceList |
ResizeFaceBuilder.face()
Returns the faces to resize, don't use it until nx502
License requirements: None. |
SelectFaceList |
ExtractFaceBuilder.facesToExtract()
Deprecated.
Deprecated in NX7.5.0. Use
ExtractFaceBuilder.objectToExtract() instead.
|
SelectFaceList |
ReplaceFaceBuilder.faceToSimplify()
Returns the face to simplify, only for simplify type, don't use it until nx502
License requirements: None. |
SelectFaceList |
LatticeBuilder.filterToolFace()
Returns the faces of the boundary body that the dangling rods connected to will be removed from the lattice body
License requirements: None. |
SelectFaceList |
SewBuilder.targetFaces()
Returns the target solid faces
License requirements: None. |
SelectFaceList |
SewBuilder.toolFaces()
Returns the tool solid faces
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
SelectFaceList |
SolidPunchBuilder.pierceFaces()
Returns the pierce faces of the tool body.
|
Modifier and Type | Method and Description |
---|---|
SelectFaceList |
ShipProfileCutoutBuilder.pierceFaces()
Returns the pierce faces
License requirements: None. |
SelectFaceList |
EndCutBuilder.placementFaces()
Returns the select placement faces.
|
SelectFaceList |
EdgeCutBuilder.selectTargetFace()
Returns the select target face.
|
Modifier and Type | Method and Description |
---|---|
SelectFaceList |
OrientationMethodBuilder.normalFaceList()
Deprecated.
Deprecated in NX12.0.0. Use
OrientationMethodBuilder.faces()
|
Modifier and Type | Method and Description |
---|---|
SelectFaceList |
TransportSurfaceBuilder.faces()
Returns the faces.
|
Modifier and Type | Method and Description |
---|---|
SelectFaceList |
OverstockFacesBuilder.faces()
Returns the faces qualified for overstock application.
|
SelectFaceList |
FittingOverstockBuilder.faces()
Returns the faces to apply overstock to.
|
Modifier and Type | Method and Description |
---|---|
SelectFaceList |
UnfoldingSimulationBuilder.bendFaces()
Returns the bend faces
License requirements: None. |
SelectFaceList |
ElectrodeInitializationBuilder.faceList()
Returns the face list whose center will be the origin of the machine set csys.
|
SelectFaceList |
ForceCalculationBuilder.forceProcess()
Returns the process used to calculate force.
|
SelectFaceList |
WallThicknessCheckerBuilder.inspectionFaces()
Returns the selected faces for displaying the thickness results on the Inspect Tab page.
|
SelectFaceList |
MoldCsysBuilder.prod()
Returns the selected faces are used to create a bounding box whose center
will be the new origin of WCS
License requirements: None. |
SelectFaceList |
MWMoldedPartValidationBuilder.regionFaces()
Returns the faces selected for assigning to the cavity or core region.
|
SelectFaceList |
DirectUnbendBuilder.selBend()
Returns the selection of bends.
|
SelectFaceList |
DirectUnfoldBuilder.selectBend()
Returns the selection list that stores bend faces.
|
SelectFaceList |
MWSearchRegionBuilder.selectBoundaryFaces()
Returns the select boundary faces
License requirements: None. |
SelectFaceList |
BendOperationBuilder.selectedBend()
Returns the selection of bends.
|
SelectFaceList |
SpecialPiercingInsertBuilder.selectFace()
Returns the select face
License requirements: None. |
SelectFaceList |
GeneralInsertBuilder.selectFace()
Returns the select face
License requirements: None. |
SelectFaceList |
BackingPadBuilder.selectFaces()
Returns the select faces
License requirements: None. |
SelectFaceList |
ElectrodeCopyBuilder.selectFromFace()
Returns the selected 'from' face
License requirements: None. |
SelectFaceList |
PiercingInsertMiniToolsBuilder.selectScrapOrInsert()
Returns the select scrap or insert for association update.
|
SelectFaceList |
PiercingInsertBuilder.selectScrapOrInsert()
Returns the select scrap or insert for association update.
|
SelectFaceList |
MWSearchRegionBuilder.selectSeedFaces()
Returns the select seed faces
License requirements: None. |
SelectFaceList |
ReplaceSolidBuilder.selFace()
Returns the selected replacement face.
|
SelectFaceList |
DirectUnfoldBuilder.selPlanarFaces()
Returns the planar faces selected as the start of automatic recognition.
|
SelectFaceList |
ElectrodeCopyBuilder.selToFace()
Returns the selected 'to' face
License requirements: None. |
SelectFaceList |
ShimBuilder.shimFace()
Returns the face for doing shim body
License requirements: None. |
SelectFaceList |
TrimSolidBuilder.taggedFaces()
Returns the faces with the defined attribute to create trim solid.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.