Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
nxopen.display |
Provides classes and interfaces for Display.
|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Interface and Description |
---|---|
interface |
CutView
Represents a Cut View
Cut Views may only be created via a Master Cut Builder. |
Modifier and Type | Method and Description |
---|---|
ModelingView |
CutViewCollection.createLinkedSectionView(CutView view)
Create a linked section view.
|
ModelingView |
ModelingViewList.findItem(int index)
Returns the object at the input index.
|
ModelingView |
ModelingViewCollection.findObject(String journalIdentifier)
Finds the
ModelingView with the given identifier
as recorded in a journal. |
ModelingView[] |
SelectModelingViewList.getArray()
Returns the list of objects in the selection list.
|
ModelingView[] |
ModelingViewList.getContents()
Gets the contents of the entire list
License requirements: None. |
ModelingView |
ModelingViewCollection.workView()
Returns the work view of the part.
|
Modifier and Type | Method and Description |
---|---|
boolean |
SelectModelingViewList.add(ModelingView object)
Adds an object to the list
License requirements: None. |
boolean |
SelectModelingViewList.add(ModelingView[] objects)
Adds a set of objects to the list
License requirements: None. |
boolean |
SelectModelingViewList.add(ModelingView selection,
View view,
Point3d point)
Adds the object with the objects view and objects point
License requirements: None. |
void |
ModelingViewList.append(ModelingView object)
Appends an object to the list
License requirements: None. |
void |
ModelingViewList.append(ModelingView[] objects)
Appends a set of objects to the list
License requirements: None. |
boolean |
SelectModelingViewList.contains(ModelingView object)
Returns whether the specified object is already in the list or not.
|
void |
ModelingViewList.erase(ModelingView obj)
Erases the object from the list, but does not delete the object.
|
void |
ModelingViewList.erase(ModelingView obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
ModelingViewList.findIndex(ModelingView obj)
Finds the index where the input object appears.
|
void |
ModelingViewList.insert(int location,
ModelingView object)
Inserts an object at the specified location
License requirements: None. |
boolean |
SelectModelingViewList.remove(InferSnapType.SnapType snapType,
ModelingView selection1,
View view1,
Point3d point1,
ModelingView selection2,
View view2,
Point3d point2)
Remove specified object from list.
|
boolean |
SelectModelingViewList.remove(ModelingView object)
Remove specified object from list.
|
boolean |
SelectModelingViewList.remove(ModelingView object,
View view)
Remove specified object from list.
|
boolean |
SelectModelingViewList.removeArray(ModelingView[] objects)
Remove specified objects from list.
|
void |
Layout.replaceView(ModelingView view,
int row,
int column,
boolean performFitView)
Replaces a
ModelingView with another one at a specified position. |
void |
Layout.replaceView(ModelingView oldView,
ModelingView newView,
boolean performFitView)
Replaces a
ModelingView with another one. |
void |
SelectModelingViewList.setArray(ModelingView[] objects)
Sets the list of objects in the selection list.
|
void |
ModelingViewList.setContents(ModelingView[] objects)
Sets the contents of the entire list.
|
boolean |
SelectModelingViewList.setValueWithCaeSetObjectInfo(ModelingView selection,
CaeObjectType.CaeSubType caeSubType,
int caeSubId)
Deprecated.
Deprecated in NX10.0.0. Use other versions of
SelectObjectList.add(nxopen.TaggedObject) .
|
boolean |
SelectModelingViewList.setValueWithSnap(InferSnapType.SnapType snapType,
ModelingView selection1,
View view1,
Point3d point1,
ModelingView selection2,
View view2,
Point3d point2)
The object being selected with the objects view and objects point and snap information.
|
void |
LayoutDefinition.setView(int row,
int column,
ModelingView view)
Sets the
ModelingView at specified position in layout. |
void |
ModelingViewList.swap(ModelingView object1,
ModelingView object2)
Exchanges the position of two objects inside the list.
|
Modifier and Type | Interface and Description |
---|---|
interface |
LightweightSectionView
Represents a PMI Lightweight Section View
Created with LightweightSection . |
interface |
SearchModelView
Represents a search model view
To create or edit an instance of this class, use SearchModelViewBuilder Created in NX7.5.0 |
Modifier and Type | Method and Description |
---|---|
ModelingView |
AnnotationManager.createQueryView(Annotation[] pmiSymbols)
Creates a model view displaying the given PMI symbols.
|
Modifier and Type | Method and Description |
---|---|
SearchModelViewBuilder |
SearchModelViewCollection.createSearchModelViewBuilder(ModelingView searchModelView)
Creates the Search PMI builder
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
ModelingView |
DynamicSectionBuilder.view()
Returns the modeling view in which section object edits are being done.
|
Modifier and Type | Method and Description |
---|---|
void |
Camera.applyToView(ModelingView view)
Applies the parameters of a camera to a view
License requirements: None. |
DynamicSectionBuilder |
DynamicSectionCollection.createSectionBuilder(DynamicSection section,
ModelingView view)
Creates a
DynamicSectionBuilder object if the section
is null. |
DynamicSectionBuilder |
DynamicSectionCollection.createSectionBuilder(ModelingView view)
Creates a
DynamicSectionBuilder object that is used
to edit a section object in the specified view. |
void |
DynamicSectionBuilder.editView(ModelingView view)
Edits the section object in the modeling view.
|
void |
DynamicSectionBuilder.setView(ModelingView view)
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
ModelingView |
DraftingViewCollection.getParentOfView(View view)
Find the parent cut (sectioned) model view of a drawing member view.
|
ModelingView |
SelectModelViewBuilder.selectedView()
Returns the selected view
License requirements: None. |
ModelingView |
AddRemoveBoxViewBuilder.selectedView()
Returns the selected view
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
BaseView |
SheetDraftingViewCollection.createBaseView(ModelingView modelView,
Point3d drawingReferencePoint,
double viewScale,
boolean inheritClippingBoundry)
For the selected part adds the base view as well as returns the reference to
DraftingView . |
void |
SelectModelViewBuilder.setSelectedView(ModelingView view)
License requirements: drafting ("DRAFTING") . |
void |
AddRemoveBoxViewBuilder.setSelectedView(ModelingView selectedView)
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
ModelingView |
MasterCutBuilder.cutView()
Returns the cut view
License requirements: solid_modeling ("SOLIDS MODELING") . |
Modifier and Type | Method and Description |
---|---|
void |
MasterCutBuilder.setCutView(ModelingView cutView)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.