public interface ModelingViewCollection extends TaggedObjectCollection
ModelingView
s.
BasePart
TaggedObjectCollection.Iterator
Modifier and Type | Method and Description |
---|---|
void |
expandCollapseModelViewNode(boolean expand)
Expand or collapse the Model View node in the Part Navigator.
|
ModelingView |
findObject(String journalIdentifier)
Finds the
ModelingView with the given identifier
as recorded in a journal. |
ModelingView |
workView()
Returns the work view of the part.
|
_find_next, iterator
ModelingView findObject(String journalIdentifier) throws NXException, RemoteException
ModelingView
with the given identifier
as recorded in a journal. An object may not return the same value as its
JournalIdentifier in different versions of the software. However,
newer versions of the software should find the same object when
FindObject is passed older versions of its journal identifier. In general,
this method should not be used in handwritten code and exists to
support record and playback of journals.
An exception will be thrown if no object can be found with the given
journal identifier.
journalIdentifier
- Identifier of the modeling view to be foundNXException
RemoteException
ModelingView workView() throws NXException, RemoteException
NXException
RemoteException
void expandCollapseModelViewNode(boolean expand) throws NXException, RemoteException
expand
- NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.