Interface | Description |
---|---|
Background |
Represents a
Background
Background defines how background pixels are displayed. |
BoundedGrid |
Represents a bounded grid
Bounded grids are not supported in KF. |
BoundedGridBuilder |
Represents the builder for creating a bounded grid
BoundedGrid . |
Camera | |
CameraBuilder |
Represents a
CameraBuilder
Cameras are not supported in KF. |
CameraCollection |
Represents a collection cameras
To obtain an instance of this class, refer to BasePart Created in NX5.0.0 |
CgfxAttr | Deprecated
Deprecated in NX10.0.0.
|
CgfxAttrCollection | Deprecated
Deprecated in NX10.0.0.
|
CgfxAttributeValueColor3Builder | Deprecated
Deprecated in NX10.0.0.
|
CgfxAttributeValueColor4Builder | Deprecated
Deprecated in NX10.0.0.
|
CgfxAttributeValueFileBuilder | Deprecated
Deprecated in NX10.0.0.
|
CgfxAttributeValueFloat3Builder | Deprecated
Deprecated in NX10.0.0.
|
CgfxAttributeValueFloat4Builder | Deprecated
Deprecated in NX10.0.0.
|
CgfxAttributeValueIntegerBuilder | Deprecated
Deprecated in NX10.0.0.
|
CgfxAttributeValueNumberBuilder | Deprecated
Deprecated in NX10.0.0.
|
CgfxMattex | Deprecated
Deprecated in NX10.0.0.
|
CgfxMattexBuilder | Deprecated
Deprecated in NX10.0.0.
|
CgfxMattexCollection | Deprecated
Deprecated in NX10.0.0.
|
DatumPlaneGrid |
Represents a grid on a datum plane
Datum plane grids are not supported in KF. |
DatumPlaneGridBuilder |
Represents the builder for adding a datum plane grid
DatumPlaneGrid
to a datum plane. |
DecalBuilder |
Represents a
DecalBuilder
This class is restricted to being called from a program running during an Interactive NX session. |
DecalCollection |
Represents a collection decal material texture
This class is restricted to being called from a program running during an Interactive NX session. |
DynamicSection |
Represents a dynamic section
To create or edit an instance of this class, use DynamicSectionBuilder Created in NX6.0.0 |
DynamicSectionBuilder |
Represents a Dynamic Section Builder used for creating sections.
|
DynamicSectionCollection |
Represents a collection of dynamic section objects
To obtain an instance of this class, refer to BasePart Created in NX6.0.0 |
DynamicSectionCut | |
DynamicSectionTypes |
Represents a enumerations used by Dynamic Section Builder.
|
EntitySelectionPlane |
Represents a grid on a datum plane
Entity selection planes are not supported in KF. |
EnvironmentBuilder |
Represents a
EnvironmentBuilder
This controls environment image, tone mapping, and stages. |
ExtractScene |
Represents a
ExtractScene
This class is restricted to being called from a program running during an Interactive NX session. |
FacetSettingsBuilder |
Represents a
FacetSettingsBuilder
Facet Settings are not supported in KF. |
GlobalIlluminationBuilder |
Represents a
GlobalIlluminationBuilder . |
Grid |
Represents a grid
Grids are not supported in KF. |
GridBuilder |
Represents the builder for adding a grid
Grid
This is an abstract class, and cannot be instantiated. |
GridCollection |
Represents a collection of plane grid objects
To obtain an instance of this class, refer to BasePart Created in NX6.0.0 |
IDynamicSectionCutCreator |
Represents a dynamic section-cut creator that generates dynamic
section-cuts (see
DynamicSectionCut ). |
Image |
Represents a
Image
This class is restricted to being called from a program running during an Interactive NX session. |
ImageBase |
Represents a
ImageBase that provides
definition, orientation, sizing, and display setting controls for image
based objects. |
ImageBaseBuilder |
Represents a
ImageBaseBuilder . |
ImageBasedLighting |
Represents a
ImageBasedLighting
Image-based Lighting (IBL) is only performed in High Quality Image
renderings. |
ImageCollection |
Represents a collection of image objects
To obtain an instance of this class, refer to BasePart Created in NX9.0.0 |
ImageData |
Represents a
ImageData that stores the
contents of a previously imported image file in the part. |
ImageDataCollection |
Represents a collection of
ImageData
objects. |
IrayPlusMaterialAttribute |
Represents an IrayPlus Attribute
This class is restricted to being called from a program running during an Interactive NX session. |
IrayPlusMaterialAttributeEnum |
Represents a IrayPlus Enum Attribute
This class is restricted to being called from a program running during an Interactive NX session. |
IrayPlusMaterialEditorBuilder |
Represents a
IrayPlusMaterialEditorBuilder
This class is restricted to being called from a program running during an Interactive NX session. |
IrayPlusSimpleMaterialEditorBuilder |
Represents a
IrayPlusSimpleMaterialEditorBuilder
This class is restricted to being called from a program running during an Interactive NX session. |
IRayPlusStudioEditorBuilder |
Represents a
IRayPlusStudioEditorBuilder . |
LayerSettingsBuilder |
Represents a builder for object layer settings.
|
LightBuilder |
Represents a
LightBuilder
This class is restricted to being called from a program running during an Interactive NX session. |
Lighting |
Represents a
Lighting
Lights are used to illuminate the scene in Shaded and Studio rendering
styles, as well as in High Quality Images. |
NonProportionalZoom |
Provides non-proportional zoom capability
To create a new instance of this class, use ViewCollection.createNonProportionalZoom() Default values. |
PerspectiveOptionsBuilder |
Represents a
PerspectiveOptionsBuilder
Cameras are not supported in KF. |
PlanarShipGrid |
Represents a planar ship grid.
|
PlanarShipGridBuilder |
Represents a
PlanarShipGrid builder. |
PlaneGrid |
Represents a grid on a bounded plane
Plane grids are not supported in KF. |
PlaneGridBuilder |
Represents the builder for adding a bounded grid
PlaneGrid
to a plane. |
PointCloud |
Represents a
PointCloud imported from point data files. |
PointCloudBuilder |
Represents a
PointCloudBuilder . |
PointCloudClippingBoxesListItemBuilder |
Represents a
PointCloudClippingBoxesListItemBuilder
to create clipping regions for PointCloud . |
PointCloudClippingBoxesListItemBuilderList |
Represents a list of objects.
|
PointCloudCollection |
Represents a collection of point cloud objects
To obtain an instance of this class, refer to BasePart Created in NX11.0.0 |
RasterImage |
Represents a
RasterImage that provides
placing an imported image onto a plane (with controls for orientation,
sizing, and display) to use as a reference in the model to create geometry. |
RasterImageBuilder |
Represents a
RasterImageBuilder . |
RayTracedStudioBuilder |
Represents a
RayTracedStudioBuilder . |
RayTracedStudioEditorBuilder |
Represents a
RayTracedStudioEditorBuilder . |
Reflection |
Represents a
Reflection
Reflection defines the source of reflection in shiny objects for Studio
rendering style or High Quality Images. |
SaveImageFileBrowserBuilder |
Represents a
SaveImageFileBrowserBuilder . |
Scene |
Represents a
Scene
A scene is comprised of background, stage, reflection, lights and
image-based lighting subobjects. |
SectionCurveSettingsBuilder | |
SelPref |
Represents a
SelPref
To obtain a instance of this class use SelPrefCollection.createSelPref() Created in NX5.0.0 |
SelPrefCollection |
Represents a collection SelPref
To obtain an instance of this class, refer to BasePart Created in NX5.0.0 |
Shadows |
Represents a
Shadows
This class is restricted to being called from a program running during an Interactive NX session. |
Stage |
Represents a
Stage
A stage is an environment cube, a six-sided room, that can have between
one and six visible walls. |
StudioImageCaptureBuilder |
Represents a
StudioImageCaptureBuilder
This class is restricted to being called from a program running during an Interactive NX session. |
TransientText |
Represents temporary text strings which can be used for Temporary Display .
|
TrueShading |
Represents a True Shading object
TrueShading is not supported in KF. |
TrueShadingBuilder |
Represents a
TrueShading builder To create a new instance of this class, use TrueShadingCollection.createTrueShadingBuilder(nxopen.display.TrueShading) Created in NX6.0.0 |
TrueShadingCollection |
Represents a collection SHED objects
To obtain an instance of this class, refer to BasePart Created in NX6.0.0 |
TrueStudio |
Represents a True Shading object
TrueStudio is not supported in KF. |
TrueStudioBuilder |
The TrueStudioBuillder manages Advanced Studio visualization display
To create a new instance of this class, use TrueStudioCollection.createTrueStudioBuilder(nxopen.display.TrueStudio) Created in NX8.0.0 |
TrueStudioCollection |
Represents a collection TrueStudio objects
To obtain an instance of this class, refer to BasePart Created in NX6.0.0 |
Wall |
Represents a
Wall
This class is restricted to being called from a program running during an Interactive NX session. |
Class | Description |
---|---|
Background.BackgroundDomeType |
dome types
|
Background.CategoryType |
background 2D3D types
|
Background.Type |
background types
|
BoundedGridBuilder.CornerPointsData |
This class holds the data returned from
BoundedGridBuilder.getCornerPoints() |
BoundedGridBuilder.LabelReferenceType |
Specifies label reference.
|
BoundedGridBuilder.ShowLabelType |
Specifies label option to be used for grid label display.
|
CameraBuilder.Aperture |
Predefined apertures: f2.8, f5.6, f8, f11, f16, f22
|
CameraBuilder.FovMeasured |
either horizontal or vertical measure
|
CameraBuilder.LensAngle |
the way to define the field of view angle
|
CameraBuilder.LensFlare |
Predefined lens flare types: Standard, 35mm, 50mm, 105mm,
polygonal, 35mm poly, 50mm poly, 105mm poly, spark, star
|
CameraBuilder.StockLens |
Predefined lenses: 28, 35, 50, 70, 105, 135, 210, 300mm
|
CameraBuilder.Types |
the camera types
|
CgfxMattexBuilder.Technique |
The technique is an index to a technique name in a list found in the CgFX file.
|
CgfxMattexBuilder.TextureSpace | Deprecated
Deprecated in NX7.5.2.
|
CgfxMattexBuilder.TextureSpaceShader |
The texture space shader type indicates the type of texture space shader to use for CgFX shader
|
CgfxMattexBuilder.UseCameraDirectionPlane |
The option indicates which texture space vectors are updated upon Update Texture to Camera Direction action
|
DatumPlaneGridBuilder.GridOrientationType |
Specifies grid orientation option to be used for grid display.
|
DecalBuilder.Anchor |
image anchor
|
DecalBuilder.DecalIllumination |
decal illumination type
|
DecalBuilder.DecalReflectivities |
decal reflectivity type
|
DecalBuilder.ImageSize |
image size type
|
DecalBuilder.Scaling |
decal scaling type
|
DynamicSectionBuilder.ActivePlaneData |
This class holds the data returned from
DynamicSectionBuilder.getActivePlane() |
DynamicSectionBuilder.AllPlanesGeometryData |
This class holds the data returned from
DynamicSectionBuilder.getAllPlanesGeometry() |
DynamicSectionBuilder.BoundingBoxData |
This class holds the data returned from
DynamicSectionBuilder.getBoundingBox() |
DynamicSectionBuilder.LoadAllIntersectingData |
This class holds the data returned from
DynamicSectionBuilder.loadAllIntersecting() |
DynamicSectionBuilder.OffsetLimitsData |
This class holds the data returned from
DynamicSectionBuilder.getOffsetLimits() |
DynamicSectionBuilder.PlaneGeometryData |
This class holds the data returned from
DynamicSectionBuilder.getPlaneGeometry(nxopen.display.DynamicSectionTypes.Axis, nxopen.display.DynamicSectionTypes.ActivePlane) |
DynamicSectionTypes.ActivePlane |
Specifies active clip plane in the active plane pair.
|
DynamicSectionTypes.Axis |
Specifies axis.
|
DynamicSectionTypes.CapColorOption |
Specifies cap color type to be used for the cap.
|
DynamicSectionTypes.Clip |
Specifies clipping type.
|
DynamicSectionTypes.CoordinateSystem |
Specifies the coordinate system used for creating
principal planes i.e.
|
DynamicSectionTypes.CurveColorOption |
Specifies the color of the curves created by the
section plane.
|
DynamicSectionTypes.Type |
Specifies different type of sectioning.
|
EnvironmentBuilder.GroundPlaneTypes |
Represents an index to a ground plane type define
|
EnvironmentBuilder.ImageBlurType |
lighting image blurr type
|
EnvironmentBuilder.ImageUpVectorTypes |
up vector type
|
EnvironmentBuilder.ToneMappingTypes |
tone mapping type - do not enable until NX11
|
FacetSettingsBuilder.AdvVisToleranceSetting |
Specifies which set of tolerances are to be used for rendering facets
for display for Advanced Visualization views.
|
FacetSettingsBuilder.FacetScale |
Denotes what type of scaling factor is applied to the corresponding tolerances used to generate facets.
|
FacetSettingsBuilder.FacetToViewRatio | Deprecated
Deprecated in NX9.0.0.
|
FacetSettingsBuilder.FacetUpdate |
Specifies whether an Update Display or Fit operation is to
regenerate the facets for only visible objects, for all objects or
for no objects.
|
FacetSettingsBuilder.ShadedToleranceSetting |
Specifies which set of tolerances are to be used for rendering facets
for display for Shaded views.
|
GridBuilder.LineStyleType |
Specifies line style to be used for major and minor lines of the grid.
|
GridBuilder.LineWeightType |
Specifies line weight to be used for major and minor lines of the grid.
|
ImageBaseBuilder.BasePointChoices |
Specifies image reference base point choice.
|
ImageBaseBuilder.CornerPointsData |
This class holds the data returned from
ImageBaseBuilder.getCornerPoints() |
ImageBaseBuilder.ImageColorModes |
Describes image color modes.
|
ImageBaseBuilder.InsertionPoint |
Describes insertion point type.
|
ImageBaseBuilder.ReferenceDirection |
Specifies image alignment reference direction type.
|
ImageBaseBuilder.SizeOptions |
Describes size options.
|
ImageBaseBuilder.TransparencyColorFrom |
Transparency Color From
|
ImageBasedLighting.ImageBlurType |
lighting image blurr type
|
ImageBasedLighting.ImagesType |
images type - environment used for generating image-based lighting
|
ImageBasedLighting.ImageUpVectorTypes |
up vector type
|
ImageBasedLighting.ShadowsType |
shadow type
|
IrayPlusMaterialEditorBuilder.AddComponentData |
This class holds the data returned from
IrayPlusMaterialEditorBuilder.addComponent(java.lang.String) |
IrayPlusMaterialEditorBuilder.ComponentInfoData |
This class holds the data returned from
IrayPlusMaterialEditorBuilder.getComponentInfo(java.lang.String) |
IrayPlusMaterialEditorBuilder.LayerType |
Layer types used in iray plus material
|
IrayPlusMaterialEditorBuilder.MaterialLayersInfoData |
This class holds the data returned from
IrayPlusMaterialEditorBuilder.getMaterialLayersInfo() |
IrayPlusSimpleMaterialEditorBuilder.TextureSpace |
texture spacee type
|
IRayPlusStudioEditorBuilder.DynamicIRayPlusStudioRenderModeType |
To specify the quality and performance of the Ray Traced Studio display when dynamic interaction stops
|
IRayPlusStudioEditorBuilder.IRayPlusStudioRemoteRenderFormatType |
To specify the Ray Traced Studio remote rendering format
|
IRayPlusStudioEditorBuilder.IRayPlusStudioRemoteRenderType |
To specify the Ray Traced Studio remote rendering type
|
IRayPlusStudioEditorBuilder.IRayPlusStudioRemoteRenderVideoType | Deprecated
Deprecated in NX12.0.0.
|
IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageFileFormatType |
To specify the Ray Traced Studio static image file format
|
IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageOrientationType |
To specify the Ray Traced Studio static image orientation
|
IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType |
To specify the Ray Traced Studio static image resolution
|
IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageSizeType |
To specify the Ray Traced Studio static image size
|
IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageUnitsType |
To specify the Ray Traced Studio static image units
|
LayerSettingsBuilder.LayerOptionType |
Specifies the layer options.
|
LightBuilder.LightMode |
light_mode
|
LightBuilder.ShadowType |
shadow types
|
NonProportionalZoom.MethodType |
Sets the kind of mouse interaction that will define the non-proportional zoom.
|
PlanarShipGridBuilder.ExtentData |
This class holds the data returned from
PlanarShipGridBuilder.getExtent() |
PlanarShipGridBuilder.IntersectOption |
Settings that indicate how to search for objects that intersect the plane.
|
PlanarShipGridBuilder.LabelDisplayOption |
Settings that indicate what grid lines should be labelled.
|
PointCloudBuilder.BrightnessModes |
Specifies point cloud brightness display mode choice.
|
PointCloudBuilder.ColorModes |
Specifies point cloud color display mode choice.
|
PointCloudClippingBoxesListItemBuilder.ClippingSides |
Specifies clipping side options used for defined clipping box.
|
RayTracedStudioBuilder.StationaryDisplayQualityType |
To specify the quality and performance of the Ray Traced Studio display.
|
RayTracedStudioEditorBuilder.DynamicRayTracedStudioTilingQualityType |
To specify the quality and performance of the interactive, dynamic Ray Traced Studio display.
|
RayTracedStudioEditorBuilder.RayTracedStudioStaticImageFileFormatType |
To specify the Ray Traced Studio static image file format
|
RayTracedStudioEditorBuilder.RayTracedStudioStaticImageOrientationType |
To specify the Ray Traced Studio static image orientation
|
RayTracedStudioEditorBuilder.RayTracedStudioStaticImageResolutionType |
To specify the Ray Traced Studio static image resolution
|
RayTracedStudioEditorBuilder.RayTracedStudioStaticImageSizeType |
To specify the Ray Traced Studio static image size
|
RayTracedStudioEditorBuilder.RayTracedStudioStaticImageUnitsType |
To specify the Ray Traced Studio static image units
|
RayTracedStudioEditorBuilder.StaticAntialiasingType |
To specify the antialiasing quality during stationary Ray Traced Studio display during static image rendering
|
RayTracedStudioEditorBuilder.StaticRayTracedStudioQualityType |
To specify the quality and performance of the Ray Traced Studio display during static image rendering
|
RayTracedStudioEditorBuilder.StationaryAntialiasingType |
To specify the antialiasing quality during stationary Ray Traced Studio display when dynamic interaction stops
|
RayTracedStudioEditorBuilder.StationaryRayTracedStudioQualityType |
To specify the quality and performance of the Ray Traced Studio display when dynamic interaction stops
|
Reflection.Type |
where the reflections for rendering will be obtained
|
SaveImageFileBrowserBuilder.FileFormats |
To specify the Ray Traced Studio static image file format
|
SectionCurveSettingsBuilder.ColorOptionType |
Specifies the color of the curves.
|
SelPref.FaceAnalysisViews |
Represents the face analysis views type
|
SelPref.Method |
Represents the chaining method type
|
SelPref.MouseGesture |
Represents the mouse gesture type
|
SelPref.SelectionRadius |
Represents the selection radius type
|
SelPref.SelectionRule |
Represents the selection rule type
|
SelPref.ShadedViews |
Represents the shaded views type
|
Shadows.RealTimeState |
Real time type settings - environment_shadow_catcher_only is enabled only in Basic Studio mode
|
Shadows.SsaoContrastType |
Shadows SSAO contrast settings
|
Shadows.SsaoQualityType |
Shadows SSAO quality settings
|
Stage.OrientationType |
Represents an index to a floor plane type define
|
Stage.WallType |
Represents an index to a particular wall in the
stage.
|
StudioImageCaptureBuilder.AASamplesEnumType |
Provide the following anti-aliasing sample size for off screen image capture
|
StudioImageCaptureBuilder.DPIEnumType |
Provide the following screen capture resolutions in dots per inch
|
StudioImageCaptureBuilder.DrawingSizeEnumType |
Provide the following standard Drawing sizes
|
StudioImageCaptureBuilder.OrientEnumType |
Provide the following options to image orientation
|
StudioImageCaptureBuilder.UnitsEnumType |
Provide the following resolution unit options to screen capture
|
TransientText.AbsoluteTextSizeData |
This class holds the data returned from
TransientText.getAbsoluteTextSize() |
TransientText.StandardTextRef |
This enumerated type specifies the type of reference point used in the text box
for standard_text methods.
|
TransientText.TextSize |
Provides a way to specify the size of the desired text, as small,
medium or large (normal is a synonym for medium).
|
TransientText.ViewType |
the view or views in which the transient text is to be displayed.
|
TrueShadingBuilder.BgdImageType |
Background image types
|
TrueShadingBuilder.BgdType |
Background colors and image types
|
TrueShadingBuilder.EnvironmentMapType |
Global environment reflection map types
|
TrueShadingBuilder.MaterialType |
Global material and per object overriding material types
|
TrueShadingBuilder.SHEDLightCollectionType |
Scene lighting collection types
|
TrueShadingBuilder.SurfaceOrientType |
Shadow plane projection orientation types
|
TrueStudioBuilder.GlobalMaterial |
Types of True Studio Global Material display.
|
TrueStudioBuilder.RenderMethod |
Types of True Studio Render Methods.
|
Wall.MaterialTextureType |
the new wall material texture type
|
Wall.MaterialType | Deprecated
Deprecated in NX10.0.0.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.