public interface CutViewCollection extends TaggedObjectCollection
Modifier and Type | Interface and Description |
---|---|
static class |
CutViewCollection.IsCutBodyOfViewData
This class holds the data returned from
isCutBodyOfView(nxopen.Body, nxopen.CutView) |
static class |
CutViewCollection.IsUncutBodyOfViewData
This class holds the data returned from
isUncutBodyOfView(nxopen.Body, nxopen.CutView) |
TaggedObjectCollection.Iterator
Modifier and Type | Method and Description |
---|---|
ModelingView |
createLinkedSectionView(CutView view)
Create a linked section view.
|
void |
deleteCutView(CutView view)
Delete the Master Cut feature associated with a cut view.
|
CutView |
findObject(String journalIdentifier)
Finds the
CutView with the given identifier
as recorded in a journal. |
DisplayableObject[] |
getCutViewsOfObject(Body body)
Find the cut views of an object.
|
boolean |
isCutBody(Body body)
Return a "true" if the body is a cut body.
|
CutViewCollection.IsCutBodyOfViewData |
isCutBodyOfView(Body body,
CutView view)
Return a "true" if the body is a cut body in the view.
|
boolean |
isToolBody(Body body)
Return a "true" if the body is a tool body.
|
CutViewCollection.IsUncutBodyOfViewData |
isUncutBodyOfView(Body body,
CutView view)
Return a "true" if the body is an uncut body in the view.
|
void |
updateCutView(CutView view)
Update the Master Cut feature associated with a cut view.
|
_find_next, iterator
CutView findObject(String journalIdentifier) throws NXException, RemoteException
CutView
with the given identifier
as recorded in a journal. An object may not return the same value as its
JournalIdentifier in different versions of the software. However,
newer versions of the software should find the same object when
FindObject is passed older versions of its journal identifier. In general,
this method should not be used in handwritten code and exists to
support record and playback of journals.
An exception will be thrown if no object can be found with the given
journal identifier.
journalIdentifier
- Identifier of the cut view to be foundNXException
RemoteException
void updateCutView(CutView view) throws NXException, RemoteException
view
- Cut viewNXException
RemoteException
void deleteCutView(CutView view) throws NXException, RemoteException
view
- Cut viewNXException
RemoteException
ModelingView createLinkedSectionView(CutView view) throws NXException, RemoteException
view
- Cut viewNXException
RemoteException
boolean isCutBody(Body body) throws NXException, RemoteException
body
- NXException
RemoteException
CutViewCollection.IsCutBodyOfViewData isCutBodyOfView(Body body, CutView view) throws NXException, RemoteException
body
- view
- Cut viewNXException
RemoteException
CutViewCollection.IsUncutBodyOfViewData isUncutBodyOfView(Body body, CutView view) throws NXException, RemoteException
body
- view
- Cut viewNXException
RemoteException
boolean isToolBody(Body body) throws NXException, RemoteException
body
- NXException
RemoteException
DisplayableObject[] getCutViewsOfObject(Body body) throws NXException, RemoteException
body
- NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.