Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Interface and Description |
---|---|
interface |
CavityMillingBuilder
Represents a CavityMilling Builder
To create a new instance of this class, use OperationCollection.createCavityMillingBuilder(nxopen.cam.CAMObject) Created in NX5.0.0 |
interface |
CenterlineDrillTurningBuilder
Represents a CenterlineDrillTurningBuilder
To create a new instance of this class, use OperationCollection.createCenterlineDrillTurningBuilder(nxopen.cam.CAMObject) Created in NX6.0.0 |
interface |
ChamferMillingBuilder
Represents a ChamferMillingBuilder Builder
To create a new instance of this class, use OperationCollection.createChamferMillingBuilder(nxopen.cam.CAMObject) Created in NX9.0.2 |
interface |
CylinderMillingBuilder
Represents a CylinderMillingBuilder Builder
To create a new instance of this class, use OperationCollection.createCylinderMillingBuilder(nxopen.cam.CAMObject) Created in NX8.0.0 |
interface |
CylindricalMillingBuilder
Represents a CylindricalMilling Builder
This is an abstract class and cannot be instantiated. |
interface |
DocumentationBuilder
Represents a Documentation Builder
To create a new instance of this class, use OperationCollection.createDocumentationBuilder(nxopen.cam.CAMObject) Created in NX9.0.3 |
interface |
EngravingBuilder
Represents a Engraving Builder
To create a new instance of this class, use OperationCollection.createEngravingBuilder(nxopen.cam.CAMObject) Created in NX5.0.0 |
interface |
FaceMillingBuilder
Represents a FaceMilling Builder
To create a new instance of this class, use OperationCollection.createFaceMillingBuilder(nxopen.cam.CAMObject) Created in NX5.0.0 |
interface |
FeatureMillingBuilder
Represents a FeatureMilling Builder
To create a new instance of this class, use OperationCollection.createFeatureMillingBuilder(nxopen.cam.CAMObject) Created in NX5.0.0 |
interface |
FinishTurningBuilder
Represents a FinishTurning Builder
To create a new instance of this class, use OperationCollection.createFinishTurningBuilder(nxopen.cam.CAMObject) Created in NX6.0.0 |
interface |
GmcOpBuilder
Represents a GmcOp Builder
To create a new instance of this class, use OperationCollection.createGmcopBuilder(nxopen.cam.CAMObject) Created in NX5.0.0 |
interface |
GrooveMillingBuilder
Represents a GrooveMillingBuilder
To create a new instance of this class, use OperationCollection.createGrooveMillingBuilder(nxopen.cam.CAMObject) Created in NX9.0.0 |
interface |
HoleDrillingBuilder
Represents a HoleDrillingBuilder Builder
To create a new instance of this class, use OperationCollection.createHoleDrillingBuilder(nxopen.cam.CAMObject) Created in NX9.0.0 |
interface |
HoleMachiningBuilder
Represents a HoleMachiningBuilder Builder
This is an abstract class and cannot be instantiated. |
interface |
HoleMakingBuilder
Represents a HoleMaking Builder
To create a new instance of this class, use OperationCollection.createHoleMakingBuilder(nxopen.cam.CAMObject) Created in NX5.0.0 |
interface |
InspectionAlignmentAssistantBuilder
Represents a CMM Inspection Alignment Assistant Builder,
this builder's Commit can produce more than one object,
the GetCommittedObjects can be used to get the objects
and the order of GetCommittedObject's output array is not stable.
|
interface |
InspectionAlignmentBuilder
Represents a CMM Inspection Alignment builder
To create a new instance of this class, use InspectionOperationCollection.createInspectionAlignmentBuilder(nxopen.cam.CAMObject) Created in NX7.5.2 |
interface |
InspectionArcFeatureBuilder
Represents a CMM Inspection Arc Feature builder
To create a new instance of this class, use InspectionOperationCollection.createInspectionArcFeatureBuilder(nxopen.cam.CAMObject) Created in NX7.0.0 |
interface |
InspectionCircleFeatureBuilder
Represents a CMM Inspection Circle Feature builder
To create a new instance of this class, use InspectionOperationCollection.createInspectionCircleFeatureBuilder(nxopen.cam.CAMObject) Created in NX7.0.0 |
interface |
InspectionCmmCommandBuilder
Represents a CMM Inspection miscellaneous command builder.
|
interface |
InspectionConeFeatureBuilder
Represents a CMM Inspection Cone Feature builder
To create a new instance of this class, use InspectionOperationCollection.createInspectionConeFeatureBuilder(nxopen.cam.CAMObject) Created in NX7.0.0 |
interface |
InspectionConstructedFeatureBuilder
Represents a CMM Inspection Constructed Feature Builder
To create a new instance of this class, use InspectionOperationCollection.createInspectionConstructedFeatureBuilder(nxopen.cam.CAMObject) Created in NX7.0.0 |
interface |
InspectionCparlnFeatureBuilder
Represents a CMM Inspection Cparln Feature Builder.
|
interface |
InspectionCurveFeatureBuilder
Represents a CMM Inspection Curve Feature builder
To create a new instance of this class, use InspectionOperationCollection.createInspectionCurveFeatureBuilder(nxopen.cam.CAMObject) Created in NX7.0.0 |
interface |
InspectionCylinderFeatureBuilder
Represents a CMM Inspection Cylinder Feature builder
To create a new instance of this class, use InspectionOperationCollection.createInspectionCylinderFeatureBuilder(nxopen.cam.CAMObject) Created in NX7.0.0 |
interface |
InspectionEdgePointFeatureBuilder
Represents a CMM Inspection Edge Point Feature builder
To create a new instance of this class, use InspectionOperationCollection.createInspectionEdgePointFeatureBuilder(nxopen.cam.CAMObject) Created in NX9.0.0 |
interface |
InspectionGraphicalReportBuilder
Represents the builder for the CMM Inspection Graphical Report Operation
To create a new instance of this class, use InspectionOperationCollection.createGraphicalReportBuilder(nxopen.cam.CAMObject) Created in NX10.0.3 |
interface |
InspectionLineFeatureBuilder
Represents a CMM Inspection Line Feature builder
To create a new instance of this class, use InspectionOperationCollection.createInspectionLineFeatureBuilder(nxopen.cam.CAMObject) Created in NX7.0.0 |
interface |
InspectionOutputOperationBuilder
this class creates the output operation
To create a new instance of this class, use InspectionOperationCollection.createInspectionOutputOperationBuilder(nxopen.cam.CAMObject) Created in NX7.0.0 |
interface |
InspectionParplnFeatureBuilder
Represents a CMM Inspection Parpln Feature Builder.
|
interface |
InspectionPathBuilder
Represents the builder for a CMM Inspection path.
|
interface |
InspectionPatternFeatureBuilder
Represents a CMM Inspection Pattern Feature builder
To create a new instance of this class, use InspectionOperationCollection.createInspectionPatternFeatureBuilder(nxopen.cam.CAMObject) Created in NX7.0.0 |
interface |
InspectionPlaneFeatureBuilder
Represents a CMM Inspection Plane Feature builder
To create a new instance of this class, use InspectionOperationCollection.createInspectionPlaneFeatureBuilder(nxopen.cam.CAMObject) Created in NX7.0.0 |
interface |
InspectionPointFeatureBuilder
Represents a CMM Inspection Point Feature builder
To create a new instance of this class, use InspectionOperationCollection.createInspectionPointFeatureBuilder(nxopen.cam.CAMObject) Created in NX7.0.0 |
interface |
InspectionSensorBuilder
Represents the builder for a CMM Inspection Sensor.
|
interface |
InspectionSphereFeatureBuilder
Represents a CMM inspection sphere feature builder
To create a new instance of this class, use InspectionOperationCollection.createInspectionSphereFeatureBuilder(nxopen.cam.CAMObject) Created in NX7.0.0 |
interface |
InspectionSurfaceFeatureBuilder
Represents a CMM Inspection Curve Feature builder
To create a new instance of this class, use InspectionOperationCollection.createInspectionSurfaceFeatureBuilder(nxopen.cam.CAMObject) Created in NX7.0.0 |
interface |
InspectionToleranceOperationBuilder
this class creates the tolerance operation
To create a new instance of this class, use InspectionOperationCollection.createInspectionToleranceOperationBuilder(nxopen.cam.CAMObject) Created in NX7.0.0 |
interface |
InspectionTorusFeatureBuilder
Represents a CMM Inspection Torus Feature builder
To create a new instance of this class, use InspectionOperationCollection.createInspectionTorusFeatureBuilder(nxopen.cam.CAMObject) Created in NX7.0.0 |
interface |
LaserTeachMode
Represents a Laser TeachMode
To create a new instance of this class, use OperationCollection.createLaserTeachMode(nxopen.cam.CAMObject) Created in NX9.0.0 |
interface |
LatheMachineControlBuilder
Represents a LatheMachineControl Builder
To create a new instance of this class, use OperationCollection.createLatheMachineControlBuilder(nxopen.cam.CAMObject) Created in NX5.0.0 |
interface |
LatheUserDefinedBuilder
Represents a LatheUserDefined Builder
To create a new instance of this class, use OperationCollection.createLatheUserDefinedBuilder(nxopen.cam.CAMObject) Created in NX5.0.0 |
interface |
ManualControlBuilder
Represents a ManualControl Operation Builder
To create a new instance of this class, use OperationCollection.createManualControlBuilder(nxopen.cam.CAMObject) Created in NX10.0.3 |
interface |
MillMachineControlBuilder
Represents a MillMachineControl Builder
To create a new instance of this class, use OperationCollection.createMillMachineControlBuilder(nxopen.cam.CAMObject) Created in NX5.0.0 |
interface |
MillOperationBuilder
Represents a MillOperation Builder
This is an abstract class and cannot be instantiated. |
interface |
MillToolProbingBuilder
Represents a Mill Tool Probing Builder
To create a new instance of this class, use OperationCollection.createMillToolProbingBuilder(nxopen.cam.CAMObject) Created in NX8.5.1 |
interface |
MillUserDefinedBuilder
Represents a MillUserDefined Builder
To create a new instance of this class, use OperationCollection.createMillUserDefinedBuilder(nxopen.cam.CAMObject) Created in NX5.0.0 |
interface |
PlanarMillingBuilder
Represents a PlanarMilling Builder
To create a new instance of this class, use OperationCollection.createPlanarMillingBuilder(nxopen.cam.CAMObject) Created in NX5.0.0 |
interface |
PlanarOperationBuilder
Represents a PlanarOperation Builder
This is an abstract class and cannot be instantiated. |
interface |
PlungeMillingBuilder
Represents a PlungeMilling Builder
To create a new instance of this class, use OperationCollection.createPlungeMillingBuilder(nxopen.cam.CAMObject) Created in NX5.0.0 |
interface |
PointToPointBuilder
Represents a Point to Point Builder (Drilling)
To create a new instance of this class, use OperationCollection.createPointToPointBuilder(nxopen.cam.CAMObject) Created in NX5.0.0 |
interface |
RadialGrooveMillingBuilder
Represents a RadialGrooveMilling Builder
To create a new instance of this class, use OperationCollection.createRadialGrooveMillingBuilder(nxopen.cam.CAMObject) Created in NX9.0.3 |
interface |
RoughFinishTurningBuilder
Represents a RoughFinishTurning Builder
This is an abstract class and cannot be instantiated. |
interface |
RoughTurningBuilder
Represents a RoughTurning Builder
To create a new instance of this class, use OperationCollection.createRoughTurningBuilder(nxopen.cam.CAMObject) Created in NX6.0.0 |
interface |
SurfaceContourBuilder
Represents a SurfaceContour Builder
To create a new instance of this class, use OperationCollection.createSurfaceContourBuilder(nxopen.cam.CAMObject) Created in NX5.0.0 |
interface |
TeachmodeTurningBuilder
Represents a TeachmodeTurningBuilder
To create a new instance of this class, use OperationCollection.createTeachmodeTurningBuilder(nxopen.cam.CAMObject) Created in NX7.5.0 |
interface |
ThreadMillingBuilder
Represents a ThreadMilling Builder
To create a new instance of this class, use OperationCollection.createThreadMillingBuilder(nxopen.cam.CAMObject) Created in NX7.5.0 |
interface |
ThreadTurningBuilder
Represents a ThreadTurning Builder
To create a new instance of this class, use OperationCollection.createThreadTurningBuilder(nxopen.cam.CAMObject) Created in NX6.0.0 |
interface |
TurningOperationBuilder
Represents a Turning Operation Builder
This is an abstract class and cannot be instantiated. |
interface |
TurnPartProbingBuilder
Represents a Turn Part Probing Builder
To create a new instance of this class, use OperationCollection.createTurnPartProbingBuilder(nxopen.cam.CAMObject) Created in NX8.5.1 |
interface |
TurnToolProbingBuilder
Represents a Turn tool probing Builder
To create a new instance of this class, use OperationCollection.createTurnToolProbingBuilder(nxopen.cam.CAMObject) Created in NX8.5.1 |
interface |
UserDefinedOprBuilder
Represents a UserDefinedOpr Builder
This is an abstract class, and cannot be instantiated. |
interface |
VazlMillingBuilder
Represents a VazlMilling Builder
To create a new instance of this class, use OperationCollection.createVazlMillingBuilder(nxopen.cam.CAMObject) Created in NX5.0.0 |
interface |
VolumeBased25DMillingOperationBuilder
Represents a VolumeBased25DMillingOperation Builder
To create a new instance of this class, use OperationCollection.createVolumeBased25dMillingOperationBuilder(nxopen.cam.CAMObject) Created in NX8.5.0 |
interface |
WedmMachineControlBuilder
Represents a WedmMachineControl Builder
To create a new instance of this class, use OperationCollection.createWedmMachineControlBuilder(nxopen.cam.CAMObject) Created in NX5.0.0 |
interface |
WedmOperationBuilder
Represents a WedmOperation Builder
To create a new instance of this class, use OperationCollection.createWedmOperationBuilder(nxopen.cam.CAMObject) Created in NX7.5.0 |
interface |
WedmUserDefinedBuilder
Represents a WedmUserDefined Builder
To create a new instance of this class, use OperationCollection.createWedmUserDefinedBuilder(nxopen.cam.CAMObject) Created in NX5.0.0 |
interface |
ZLevelMillingBuilder
Represents a ZLevelMilling Builder
To create a new instance of this class, use OperationCollection.createZlevelMillingBuilder(nxopen.cam.CAMObject) Created in NX5.0.0 |
Modifier and Type | Method and Description |
---|---|
void |
CAMSetup.trimToolPath(OperationBuilder operationBuilder)
Interactive Tool Path Trim
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.