TrimAndExtendBuilder Class¶
-
class
NXOpen.Features.
TrimAndExtendBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.TrimAndExtend
builderTo create a new instance of this class, use
NXOpen.Features.TrimFeatureCollection.CreateTrimAndExtendBuilder()
Default values.
Property Value ArrowSideOption Retain BodyOutputOption ExtendOriginalSheet CombineOption true CopyOriginalOption false Operation UntilSelected SurfaceShapeOption NaturalCurvature New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ArrowSideOption | Returns or sets the trim extend desired result type |
BodyOutputOption | Returns or sets the body output type |
CombineOption | Returns or sets the combine option determines if two bodies that make a corner are combined into one body. |
CopyOriginalOption | Returns or sets the copy original logical determines if the original body is modified or if a copy of the original is modified. |
DistanceTolerance | Returns or sets the distance tolerance |
Operation | Returns or sets the trim extend type |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ReverseTarget | Returns or sets the target reverse side flag |
ReverseTool | Returns or sets the tool reverse side flag |
SurfaceShapeOption | Returns or sets the extension method |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TargetSelection | Returns the target collector which contains either edge or face |
ToolSelection | Returns the tool collector which contains either edges or faces |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TrimAndExtendBuilderArrowSideType Enumeration | Trim or Extend Arrow Side Results type. |
TrimAndExtendBuilderOperationType Enumeration | Trim or Extend operation type. |
Property Detail¶
ArrowSideOption¶
-
TrimAndExtendBuilder.
ArrowSideOption
¶ Returns or sets the trim extend desired result type
-------------------------------------
Getter Method
Signature
ArrowSideOption
Returns: Return type: NXOpen.Features.TrimAndExtendBuilderArrowSideType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ArrowSideOption
Parameters: arrowSideType ( NXOpen.Features.TrimAndExtendBuilderArrowSideType
) –New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
BodyOutputOption¶
-
TrimAndExtendBuilder.
BodyOutputOption
¶ Returns or sets the body output type
-------------------------------------
Getter Method
Signature
BodyOutputOption
Returns: Return type: NXOpen.Features.ExtendSheetBuilderBodyOutput
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BodyOutputOption
Parameters: bodyOutputOption ( NXOpen.Features.ExtendSheetBuilderBodyOutput
) –New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CombineOption¶
-
TrimAndExtendBuilder.
CombineOption
¶ Returns or sets the combine option determines if two bodies that make a corner are combined into one body.
Applicable only for TrimExtendType of MakeCorner.
-------------------------------------
Getter Method
Signature
CombineOption
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CombineOption
Parameters: combine (bool) – New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CopyOriginalOption¶
-
TrimAndExtendBuilder.
CopyOriginalOption
¶ Returns or sets the copy original logical determines if the original body is modified or if a copy of the original is modified.
-------------------------------------
Getter Method
Signature
CopyOriginalOption
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CopyOriginalOption
Parameters: copyOriginal (bool) – New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
DistanceTolerance¶
-
TrimAndExtendBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance
-------------------------------------
Getter Method
Signature
DistanceTolerance
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance
Parameters: tolerance (float) – New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Operation¶
-
TrimAndExtendBuilder.
Operation
¶ Returns or sets the trim extend type
-------------------------------------
Getter Method
Signature
Operation
Returns: Return type: NXOpen.Features.TrimAndExtendBuilderOperationType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Operation
Parameters: operation ( NXOpen.Features.TrimAndExtendBuilderOperationType
) –New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ReverseTarget¶
-
TrimAndExtendBuilder.
ReverseTarget
¶ Returns or sets the target reverse side flag
-------------------------------------
Getter Method
Signature
ReverseTarget
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseTarget
Parameters: reverseTarget (bool) – New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ReverseTool¶
-
TrimAndExtendBuilder.
ReverseTool
¶ Returns or sets the tool reverse side flag
-------------------------------------
Getter Method
Signature
ReverseTool
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseTool
Parameters: reverseTool (bool) – New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SurfaceShapeOption¶
-
TrimAndExtendBuilder.
SurfaceShapeOption
¶ Returns or sets the extension method
-------------------------------------
Getter Method
Signature
SurfaceShapeOption
Returns: Return type: NXOpen.Features.ExtendSheetBuilderSurfaceShape
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SurfaceShapeOption
Parameters: surfaceShapeOption ( NXOpen.Features.ExtendSheetBuilderSurfaceShape
) –New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
TargetSelection¶
-
TrimAndExtendBuilder.
TargetSelection
¶ Returns the target collector which contains either edge or face
-------------------------------------
Getter Method
Signature
TargetSelection
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
ToolSelection¶
-
TrimAndExtendBuilder.
ToolSelection
¶ Returns the tool collector which contains either edges or faces
-------------------------------------
Getter Method
Signature
ToolSelection
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
TrimAndExtendBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.