TrimAndExtendBuilderOperationType Enumeration

NXOpen.Features.TrimAndExtendBuilder.OperationType is an alias for NXOpen.Features.TrimAndExtendBuilderOperationType

class NXOpen.Features.TrimAndExtendBuilderOperationType

Bases: object

Trim or Extend operation type.

Enum Members

Enum Member Enum Member Description
UntilSelected
MakeCorner
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.