ExtendSheetBuilderBodyOutput Enumeration

NXOpen.Features.ExtendSheetBuilder.BodyOutput is an alias for NXOpen.Features.ExtendSheetBuilderBodyOutput

class NXOpen.Features.ExtendSheetBuilderBodyOutput

Bases: object

Creates extension as an existing or a new entity

Enum Members

Enum Member Enum Member Description
ExtendOriginalSheet
ExtendasNewFace
ExtendasNewSheet
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.