TrimAndExtendBuilderArrowSideType Enumeration

NXOpen.Features.TrimAndExtendBuilder.ArrowSideType is an alias for NXOpen.Features.TrimAndExtendBuilderArrowSideType

class NXOpen.Features.TrimAndExtendBuilderArrowSideType

Bases: object

Trim or Extend Arrow Side Results type.

Enum Members

Enum Member Enum Member Description
Retain
Delete
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.