DrawBeadBuilder Class¶
-
class
NXOpen.Die.
DrawBeadBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a builder that is used to create or edit a
NXOpen.Die.DrawBead
feature.To create a new instance of this class, use
NXOpen.Die.DieCollection.CreateDrawBeadBuilder()
Default values.
Property Value BaseOrientation Vertical BuildEndTaper 1 BuildStartTaper 1 CenterlineProjection DrawDirection Clearance.Value 0.2 (millimeters part), 0.008 (inches part) EndPoint.InputType SelectLocation EndTaper.TaperRadius.Value 90 (millimeters part), 3.8 (inches part) EndTaper.TaperType Spherical EndTaper.TaperWashoutHeight.Value 10 (millimeters part), 0.4 (inches part) EndTaper.TaperWashoutLength.Value 50 (millimeters part), 2 (inches part) FemaleDepthType Derived FemaleDepthValue.Value 11 (millimeters part), 0.43 (inches part) FemaleWidthType Derived FemaleWidthValue.Value 12.4 (millimeters part), 0.488 (inches part) GenerateHeightCurve 0 MachineOffset 0 MaleBeadPosition Upper MetalThickness.Value 1 (millimeters part), 0.04 (inches part) OrientSectionToDraw DrawDirection Output Male TaperBead 0 TransitionDefinition Automatic New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angle tolerance. |
BaseOrientation | Returns or sets the orientation used to construct the sections representing the bead shape. |
BuildEndTaper | Returns or sets the indication if the taper at the end of the bead should be built. |
BuildStartTaper | Returns or sets the indication if the taper at the start of the bead should be built. |
Centerline | Returns the section containing the centerline of the bead. |
CenterlineProjection | Returns or sets the projection method to apply to the centerline to place it on the sewn faces. |
Clearance | Returns the expression containing the clearance value between the male and female bead sheets. |
DistanceTolerance | Returns or sets the distance tolerance. |
DrawDirection | Returns the draw direction. |
EndPoint | Returns the point location defining the end of the centerline. |
EndTaper | Returns the taper definition at the end of the bead. |
FemaleDepthType | Returns or sets the method used to calculate the female depth. |
FemaleDepthValue | Returns the expression containing the female depth value. |
FemaleFaceAttribute | Returns the attribute definition to be applied to the faces of the female bead sheet body. |
FemaleSheetAttribute | Returns the attribute definition to be applied to the female bead sheet body. |
FemaleWidthType | Returns or sets the method used to calculate the female width. |
FemaleWidthValue | Returns the expression containing the female width value. |
GenerateHeightCurve | Returns or sets the indication if the height curve should be generated. |
MachineOffset | Returns or sets the indication if the male and female output bodies are to be built with machining. |
MachiningOffsetTitleAttribute | Returns the title of the real attribute to be applied to the male and female bodies. |
MaleBeadPosition | Returns or sets the casting in which to create the male bead. |
MaleFaceAttribute | Returns the attribute definition to be applied to the faces of the male bead sheet body. |
MaleSheetAttribute | Returns the attribute definition to be applied to the male bead sheet body. |
MetalThickness | Returns the expression containing the sheet metal thickness value. |
OrientSectionToDraw | Returns or sets the method used to orient the section dimensions. |
Output | Returns or sets the output to be constructed by the draw bead feature. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PlacementFace | Returns the collector containing faces (which will sew together) that identifies the surface shape the bead is attached too. |
ReferenceDirection | Returns or sets the indication if the Left direction for section orientation should be reversed from the default direction. |
ReverseMetalThickness | Returns or sets the indication if the thickness of the sheet metal should be the same as the sewn face normals. |
SegmentList | Returns the list of NXOpen.Die.DrawBeadSegmentBuilder defining the bead sections along the centerline. |
SheetMetalFaceAttribute | Returns the attribute definition to be applied to the faces of the sheet metal sheet body. |
SheetMetalSheetAttribute | Returns the attribute definition to be applied to the sheet metal sheet body. |
StartPoint | Returns the point location defining the start of the centerline. |
StartTaper | Returns the taper definition at the start of the bead. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TaperBead | Returns or sets the indication if the bead should allow taper to be added to the side walls. |
TransitionDefinition | Returns or sets the method used to build the transition between segments. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
CreateDrawBeadSegment | Creates a NXOpen.Die.DrawBeadSegmentBuilder builder. |
CreateSegmentsFromCenterlineCurves | For each curve of the centerline, create a bead segment. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetMoreDetails | Get the detailed description strings of the draw bead. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetDefaultDrawDirection | Set the default draw direction to the -Z direction of the work coordinate system. |
SetMoreDetails | Set the detailed description strings of the draw bead. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DrawBeadBuilderFemaleDepthTypes Enumeration | Specifies how the female depth is calculated or defined. |
DrawBeadBuilderFemaleWidthTypes Enumeration | Specifies how the feamle width is calcualted or defined. |
DrawBeadBuilderMaleBeadPositionTypes Enumeration | Identifes which casting the male bead is created in. |
DrawBeadBuilderOrientSectionToDrawTypes Enumeration | Specifies if the segment height section parameter should be oriented to the draw direction or the sheet metal normal at the section location. |
DrawBeadBuilderOrientationTypes Enumeration | Identifies the orientation of the base parameters to the sheet metal. |
DrawBeadBuilderOutputTypes Enumeration | Specifies what type of output is desired for the feature creation. |
DrawBeadBuilderProjectionDirectionTypes Enumeration | Identifes how the centerline should be projected to the placement face during processing. |
DrawBeadBuilderTransitionDefinitionTypes Enumeration | Specifies how the transition area should be determined from segment to segment within a single bead. |
Property Detail¶
AngleTolerance¶
-
DrawBeadBuilder.
AngleTolerance
¶ Returns or sets the angle tolerance.
-------------------------------------
Getter Method
Signature
AngleTolerance
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleTolerance
Parameters: angleTolerance (float) – New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
BaseOrientation¶
-
DrawBeadBuilder.
BaseOrientation
¶ Returns or sets the orientation used to construct the sections representing the bead shape.
-------------------------------------
Getter Method
Signature
BaseOrientation
Returns: Return type: NXOpen.Die.DrawBeadBuilderOrientationTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BaseOrientation
Parameters: baseOrientation ( NXOpen.Die.DrawBeadBuilderOrientationTypes
) –New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
BuildEndTaper¶
-
DrawBeadBuilder.
BuildEndTaper
¶ Returns or sets the indication if the taper at the end of the bead should be built.
True indicates that the taper at the end of the bead should be created.
-------------------------------------
Getter Method
Signature
BuildEndTaper
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BuildEndTaper
Parameters: buildEndTaper (bool) – New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
BuildStartTaper¶
-
DrawBeadBuilder.
BuildStartTaper
¶ Returns or sets the indication if the taper at the start of the bead should be built.
True indicates that the taper at the start of the bead should be created.
-------------------------------------
Getter Method
Signature
BuildStartTaper
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BuildStartTaper
Parameters: buildStartTaper (bool) – New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Centerline¶
-
DrawBeadBuilder.
Centerline
¶ Returns the section containing the centerline of the bead.
-------------------------------------
Getter Method
Signature
Centerline
Returns: Return type: NXOpen.Section
New in version NX7.5.0.
License requirements: None.
CenterlineProjection¶
-
DrawBeadBuilder.
CenterlineProjection
¶ Returns or sets the projection method to apply to the centerline to place it on the sewn faces.
-------------------------------------
Getter Method
Signature
CenterlineProjection
Returns: Return type: NXOpen.Die.DrawBeadBuilderProjectionDirectionTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CenterlineProjection
Parameters: centerlineProjection ( NXOpen.Die.DrawBeadBuilderProjectionDirectionTypes
) –New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Clearance¶
-
DrawBeadBuilder.
Clearance
¶ Returns the expression containing the clearance value between the male and female bead sheets.
-------------------------------------
Getter Method
Signature
Clearance
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
DistanceTolerance¶
-
DrawBeadBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance.
-------------------------------------
Getter Method
Signature
DistanceTolerance
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance
Parameters: distanceTolerance (float) – New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
DrawDirection¶
-
DrawBeadBuilder.
DrawDirection
¶ Returns the draw direction.
-------------------------------------
Getter Method
Signature
DrawDirection
Returns: Return type: NXOpen.Die.DieDirectionBuilder
New in version NX7.5.0.
License requirements: None.
EndPoint¶
-
DrawBeadBuilder.
EndPoint
¶ Returns the point location defining the end of the centerline.
-------------------------------------
Getter Method
Signature
EndPoint
Returns: Return type: NXOpen.Die.DieLocationBuilder
New in version NX7.5.0.
License requirements: None.
EndTaper¶
-
DrawBeadBuilder.
EndTaper
¶ Returns the taper definition at the end of the bead.
-------------------------------------
Getter Method
Signature
EndTaper
Returns: Return type: NXOpen.Die.DrawBeadTaperBuilder
New in version NX7.5.0.
License requirements: None.
FemaleDepthType¶
-
DrawBeadBuilder.
FemaleDepthType
¶ Returns or sets the method used to calculate the female depth.
Only valid when taper bead is false.
-------------------------------------
Getter Method
Signature
FemaleDepthType
Returns: Return type: NXOpen.Die.DrawBeadBuilderFemaleDepthTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FemaleDepthType
Parameters: femaleDepthType ( NXOpen.Die.DrawBeadBuilderFemaleDepthTypes
) –New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
FemaleDepthValue¶
-
DrawBeadBuilder.
FemaleDepthValue
¶ Returns the expression containing the female depth value.
Only valid when taper bead is false and type is
NXOpen.Die.DrawBeadBuilderFemaleDepthTypes.Constant
.-------------------------------------
Getter Method
Signature
FemaleDepthValue
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
FemaleFaceAttribute¶
-
DrawBeadBuilder.
FemaleFaceAttribute
¶ Returns the attribute definition to be applied to the faces of the female bead sheet body.
-------------------------------------
Getter Method
Signature
FemaleFaceAttribute
Returns: Return type: NXOpen.Die.DieAttributesBuilder
New in version NX7.5.0.
License requirements: None.
FemaleSheetAttribute¶
-
DrawBeadBuilder.
FemaleSheetAttribute
¶ Returns the attribute definition to be applied to the female bead sheet body.
-------------------------------------
Getter Method
Signature
FemaleSheetAttribute
Returns: Return type: NXOpen.Die.DieAttributesBuilder
New in version NX7.5.0.
License requirements: None.
FemaleWidthType¶
-
DrawBeadBuilder.
FemaleWidthType
¶ Returns or sets the method used to calculate the female width.
Changing this will affect all segments. Only valid when taper bead is false.
-------------------------------------
Getter Method
Signature
FemaleWidthType
Returns: Return type: NXOpen.Die.DrawBeadBuilderFemaleWidthTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FemaleWidthType
Parameters: femaleWidthType ( NXOpen.Die.DrawBeadBuilderFemaleWidthTypes
) –New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
FemaleWidthValue¶
-
DrawBeadBuilder.
FemaleWidthValue
¶ Returns the expression containing the female width value.
Only valid when taper bead is false and type is
NXOpen.Die.DrawBeadBuilderFemaleWidthTypes.Constant
.-------------------------------------
Getter Method
Signature
FemaleWidthValue
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
GenerateHeightCurve¶
-
DrawBeadBuilder.
GenerateHeightCurve
¶ Returns or sets the indication if the height curve should be generated.
True if the height curve should be generated and kept.
-------------------------------------
Getter Method
Signature
GenerateHeightCurve
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GenerateHeightCurve
Parameters: generateHeightCurve (bool) – New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
MachineOffset¶
-
DrawBeadBuilder.
MachineOffset
¶ Returns or sets the indication if the male and female output bodies are to be built with machining.
Only valid when taper bead is true.
-------------------------------------
Getter Method
Signature
MachineOffset
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MachineOffset
Parameters: machineOffset (bool) – New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
MachiningOffsetTitleAttribute¶
-
DrawBeadBuilder.
MachiningOffsetTitleAttribute
¶ Returns the title of the real attribute to be applied to the male and female bodies.
The value of the attribute specifies the machining offset value to be applied. The value is derived during feature construction.
-------------------------------------
Getter Method
Signature
MachiningOffsetTitleAttribute
Returns: Return type: NXOpen.Die.DieAttributesBuilder
New in version NX7.5.0.
License requirements: None.
MaleBeadPosition¶
-
DrawBeadBuilder.
MaleBeadPosition
¶ Returns or sets the casting in which to create the male bead.
-------------------------------------
Getter Method
Signature
MaleBeadPosition
Returns: Return type: NXOpen.Die.DrawBeadBuilderMaleBeadPositionTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaleBeadPosition
Parameters: maleBeadPosition ( NXOpen.Die.DrawBeadBuilderMaleBeadPositionTypes
) –New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
MaleFaceAttribute¶
-
DrawBeadBuilder.
MaleFaceAttribute
¶ Returns the attribute definition to be applied to the faces of the male bead sheet body.
-------------------------------------
Getter Method
Signature
MaleFaceAttribute
Returns: Return type: NXOpen.Die.DieAttributesBuilder
New in version NX7.5.0.
License requirements: None.
MaleSheetAttribute¶
-
DrawBeadBuilder.
MaleSheetAttribute
¶ Returns the attribute definition to be applied to the male bead sheet body.
-------------------------------------
Getter Method
Signature
MaleSheetAttribute
Returns: Return type: NXOpen.Die.DieAttributesBuilder
New in version NX7.5.0.
License requirements: None.
MetalThickness¶
-
DrawBeadBuilder.
MetalThickness
¶ Returns the expression containing the sheet metal thickness value.
-------------------------------------
Getter Method
Signature
MetalThickness
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
OrientSectionToDraw¶
-
DrawBeadBuilder.
OrientSectionToDraw
¶ Returns or sets the method used to orient the section dimensions.
-------------------------------------
Getter Method
Signature
OrientSectionToDraw
Returns: Return type: NXOpen.Die.DrawBeadBuilderOrientSectionToDrawTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrientSectionToDraw
Parameters: orientSectionToDraw ( NXOpen.Die.DrawBeadBuilderOrientSectionToDrawTypes
) –New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Output¶
-
DrawBeadBuilder.
Output
¶ Returns or sets the output to be constructed by the draw bead feature.
-------------------------------------
Getter Method
Signature
Output
Returns: Return type: NXOpen.Die.DrawBeadBuilderOutputTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Output
Parameters: output ( NXOpen.Die.DrawBeadBuilderOutputTypes
) –New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
PlacementFace¶
-
DrawBeadBuilder.
PlacementFace
¶ Returns the collector containing faces (which will sew together) that identifies the surface shape the bead is attached too.
-------------------------------------
Getter Method
Signature
PlacementFace
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
ReferenceDirection¶
-
DrawBeadBuilder.
ReferenceDirection
¶ Returns or sets the indication if the “Left” direction for section orientation should be reversed from the default direction.
The default direction is determined by the cross of the centerline tangency and the draw direction. True indicates that the default calculation should be reversed.
-------------------------------------
Getter Method
Signature
ReferenceDirection
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceDirection
Parameters: referenceDirection (bool) – New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
ReverseMetalThickness¶
-
DrawBeadBuilder.
ReverseMetalThickness
¶ Returns or sets the indication if the thickness of the sheet metal should be the same as the sewn face normals.
True indicates that the sheet will be thickened in the same direction as the sewn face normals.
-------------------------------------
Getter Method
Signature
ReverseMetalThickness
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseMetalThickness
Parameters: reverseMetalThickness (bool) – New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
SegmentList¶
-
DrawBeadBuilder.
SegmentList
¶ Returns the list of
NXOpen.Die.DrawBeadSegmentBuilder
defining the bead sections along the centerline.-------------------------------------
Getter Method
Signature
SegmentList
Returns: Return type: NXOpen.Die.DrawBeadSegmentBuilderList
New in version NX7.5.0.
License requirements: None.
SheetMetalFaceAttribute¶
-
DrawBeadBuilder.
SheetMetalFaceAttribute
¶ Returns the attribute definition to be applied to the faces of the sheet metal sheet body.
-------------------------------------
Getter Method
Signature
SheetMetalFaceAttribute
Returns: Return type: NXOpen.Die.DieAttributesBuilder
New in version NX7.5.0.
License requirements: None.
SheetMetalSheetAttribute¶
-
DrawBeadBuilder.
SheetMetalSheetAttribute
¶ Returns the attribute definition to be applied to the sheet metal sheet body.
-------------------------------------
Getter Method
Signature
SheetMetalSheetAttribute
Returns: Return type: NXOpen.Die.DieAttributesBuilder
New in version NX7.5.0.
License requirements: None.
StartPoint¶
-
DrawBeadBuilder.
StartPoint
¶ Returns the point location defining the start of the centerline.
-------------------------------------
Getter Method
Signature
StartPoint
Returns: Return type: NXOpen.Die.DieLocationBuilder
New in version NX7.5.0.
License requirements: None.
StartTaper¶
-
DrawBeadBuilder.
StartTaper
¶ Returns the taper definition at the start of the bead.
-------------------------------------
Getter Method
Signature
StartTaper
Returns: Return type: NXOpen.Die.DrawBeadTaperBuilder
New in version NX7.5.0.
License requirements: None.
TaperBead¶
-
DrawBeadBuilder.
TaperBead
¶ Returns or sets the indication if the bead should allow taper to be added to the side walls.
Changing this will affect all segments and may affect the transition definition and output.
-------------------------------------
Getter Method
Signature
TaperBead
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TaperBead
Parameters: taperBead (bool) – New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
TransitionDefinition¶
-
DrawBeadBuilder.
TransitionDefinition
¶ Returns or sets the method used to build the transition between segments.
Changing this will affect all segments.
-------------------------------------
Getter Method
Signature
TransitionDefinition
Returns: Return type: NXOpen.Die.DrawBeadBuilderTransitionDefinitionTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TransitionDefinition
Parameters: transitionDefinition ( NXOpen.Die.DrawBeadBuilderTransitionDefinitionTypes
) –New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Method Detail¶
CreateDrawBeadSegment¶
-
DrawBeadBuilder.
CreateDrawBeadSegment
¶ Creates a
NXOpen.Die.DrawBeadSegmentBuilder
builder.Signature
CreateDrawBeadSegment()
Returns: Return type: NXOpen.Die.DrawBeadSegmentBuilder
New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
CreateSegmentsFromCenterlineCurves¶
-
DrawBeadBuilder.
CreateSegmentsFromCenterlineCurves
¶ For each curve of the centerline, create a bead segment.
Signature
CreateSegmentsFromCenterlineCurves()
New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
GetMoreDetails¶
-
DrawBeadBuilder.
GetMoreDetails
¶ Get the detailed description strings of the draw bead.
Signature
GetMoreDetails()
Returns: Array of detail strings. Return type: list of str New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
SetDefaultDrawDirection¶
-
DrawBeadBuilder.
SetDefaultDrawDirection
¶ Set the default draw direction to the -Z direction of the work coordinate system.
Signature
SetDefaultDrawDirection()
New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
SetMoreDetails¶
-
DrawBeadBuilder.
SetMoreDetails
¶ Set the detailed description strings of the draw bead.
Signature
SetMoreDetails(strings)
Parameters: strings (list of str) – Array of detail strings. New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Validate¶
-
DrawBeadBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.