DrawBeadBuilderFemaleDepthTypes Enumeration¶
NXOpen.Die.DrawBeadBuilder.FemaleDepthTypes is an alias for NXOpen.Die.DrawBeadBuilderFemaleDepthTypes
-
class
NXOpen.Die.
DrawBeadBuilderFemaleDepthTypes
¶ Bases:
object
Specifies how the female depth is calculated or defined.
Enum Members
Enum Member Enum Member Description Derived The female depth is derived from the male bead (Max Male Depth + Constant). Constant The female depth is a user specified constant. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-