DrawBeadBuilderMaleBeadPositionTypes Enumeration¶
NXOpen.Die.DrawBeadBuilder.MaleBeadPositionTypes is an alias for NXOpen.Die.DrawBeadBuilderMaleBeadPositionTypes
-
class
NXOpen.Die.
DrawBeadBuilderMaleBeadPositionTypes
¶ Bases:
object
Identifes which casting the male bead is created in.
Enum Members
Enum Member Enum Member Description Upper Attach the male bead to the upper die casting. Lower Attach the male bead to the lower die casting. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-