DrawBeadBuilderFemaleWidthTypes Enumeration¶
NXOpen.Die.DrawBeadBuilder.FemaleWidthTypes is an alias for NXOpen.Die.DrawBeadBuilderFemaleWidthTypes
-
class
NXOpen.Die.
DrawBeadBuilderFemaleWidthTypes
¶ Bases:
object
Specifies how the feamle width is calcualted or defined.
Enum Members
Enum Member Enum Member Description Derived The female width is derived from the male (Male Width + 2(Sheet Metal Thickness + Clearance)). Constant The female width is a user specified constant. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-