DrawBeadBuilderProjectionDirectionTypes Enumeration¶
NXOpen.Die.DrawBeadBuilder.ProjectionDirectionTypes is an alias for NXOpen.Die.DrawBeadBuilderProjectionDirectionTypes
-
class
NXOpen.Die.
DrawBeadBuilderProjectionDirectionTypes
¶ Bases:
object
Identifes how the centerline should be projected to the placement face during processing.
Enum Members
Enum Member Enum Member Description DrawDirection Project the centerline along the draw direction vector. NormalToPlacementFace Project the centerline along the placement face normal. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-