MillCutParameters Class¶
-
class
NXOpen.CAM.
MillCutParameters
¶ Bases:
NXOpen.CAM.CutParameters
Represents a
NXOpen.CAM.MillCutParameters
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AcrossVoids | Returns the across voids |
ActionWhenGouging | Returns or sets the action when gouging |
AdjacentBlades | Returns or sets the Adjacent Blades Stock Option Type |
AllowUndercutting | Returns or sets the allow undercutting toggle |
ApplyToLastPass | Returns or sets the status for doing Blank Sensitive finish on the last cut level |
BladeStock | Returns the blade stock |
BlankDistance | Returns the blank distance |
BlankOverhang | Returns the blank overhang (inheritable tool dependent). |
BlankStock | Returns the blank stock |
BlendStock | Returns the blend stock |
BoundaryApproximation | Returns or sets the boundary approximation toggle |
BoundaryInTol | Returns or sets the boundary intol |
BoundaryOutTol | Returns or sets the boundary out tol |
BoundaryStock | Returns or sets the boundary stock |
CheckIpwCollisions | Returns or sets the value to Check for Ipw Collsions |
CheckSafeClearance | Returns the Check Safe Clearance |
CheckStock | Returns the check stock |
CleanupOutput | Returns the Cleanup Output |
CleanupSettings | Returns the Cleanup Settings |
CornerControl | Returns the corner control |
CornerFindingOptions | Returns or sets the Corner Finding Options |
CutAngle | Returns the cut angle |
CutAreaExtensionDistance | Returns the cut area extension distance builder |
CutBelowOverhangingBlank | Returns or sets the Cut Below Overhanging Blank Method |
CutBelowToolContact | Returns or sets the cut below tool contact setting |
CutBetweenLevels | Returns or sets the cut between levels |
CutDirection | Returns the cut direction |
CutOrder | Returns or sets the cut order |
CutWallsOnly | Returns or sets the Cut Walls Only toggle |
ExtendAcrossUndercut | Returns or sets the extend across undercut toggle |
ExtendAtEdges | Returns the Extend At Edges |
ExtendFloorTo | Returns or sets the extend floor to |
ExtendToPart | Returns or sets the extend to part flag |
FinishPasses | Returns the finish passes |
FloorSameAsPartStock | Returns or sets the floor same as part stock |
FloorStock | Returns the floor stock |
FollowCheck | Returns or sets the follow check geometry status |
FromLeadingEdge | Returns the from leading edge |
FromTrailingEdge | Returns the from trailing edge |
GlobalOptimization | Returns or sets the global optimzation status |
HolderClearance | Returns the Holder Clearance |
HubStock | Returns the hub stock |
IncludeBodiesOfSurfaceRegion | Returns or sets the flag to check bodies of surface region |
IpwType | Returns or sets the IPW type |
LevelToLevel | Returns the Level to Level |
LowerLimit | Returns the lower limit |
MaxCutStep | Returns the maximum cut step |
MaxCutTraverse | Returns the max cut traverse |
MergeDistance | Returns the merge distance builder (tool dependent double) |
MinCutVolume | Returns the minimum cut volume |
MinMaterialThickness | Returns the minimum material thickness |
MinimizeNumberOfEngages | Returns or sets the minimize number of engages toggle |
MultiDepthCut | Returns the Multi Depth Cut |
NeckClearance | Returns the Neck Clearance |
OutputUncutRegions | Returns the output uncut regions |
PartSafeClearance | Returns the Part Safe Clearance |
PartStock | Returns the part stock |
PartStockOffset | Returns the part stock offset |
PatternDirection | Returns or sets the pattern direction |
PlungeDirection | Returns or sets the plunge direction |
PreventUndercutting | Returns or sets the prevent undercutting toggle |
RegionConnection | Returns or sets the region connection |
RegionSequencing | Returns or sets the region resequencing |
RollToolOverEdges | Returns or sets the roll tool over edges toggle |
RotaryMaxAngleLimit | Returns or sets the rotary max angle limit |
RotaryMinAngleLimit | Returns or sets the min angle from part axis |
SelfIntersection | Returns or sets the Standard Drive Self-Intersect Status |
ShankClearance | Returns the Shank Clearance |
ShroudStock | Returns the shroud stock |
SimplifyShapes | Returns or sets the Simplify Shapes Method |
SinglePassOffset | Returns the Single Pass Offset |
SmallAreaAvoidance | Returns the small area avoidance |
SteepContainment | Returns the steep containment |
Stepover | Returns the stepover |
StepoverLimit | Returns the Stepover Limit |
Tag | Returns the Tag for this object. |
TextDepth | Returns the Text Depth |
TlaxisBladeRollAngle | Returns or sets the max blade roll angle |
Tolerances | Returns the Tolerances builder |
TolerantMachining | Returns or sets the tolerant machining status |
ToolAxisChange | Returns the tool axis change |
ToolAxisSmoothing | Returns or sets the degree of tool axis smoothing |
ToolAxisTilt | Returns the tool axis tilt |
ToolRunOff | Returns the Tool Run Off |
ToolRunOffType | Returns or sets the Tool Run Off Type |
ToolRunOn | Returns the Tool Run On |
ToolpathSmoothing | Returns or sets the degree of tool path smoothing |
TraverseOpenPasses | Returns or sets the open passes |
TrimControl | Returns or sets the trim control method type |
TrimStock | Returns the trim stock |
TrochoidalSettings | Returns the Trochoidal Settings |
UpDownCutting | Returns the up down cutting |
UsePrevious2dIpw | Returns or sets the use previous IPW toggle |
UseToolHolder | Returns or sets the use tool holder |
ValleyOverlapDistance | Returns the valley overlap distance |
WallStock | Returns the wall stock |
ZAxisSmoothing | Returns the Z Axis Smoothing. |
Methods¶
Property Detail¶
AcrossVoids¶
-
MillCutParameters.
AcrossVoids
¶ Returns the across voids
-------------------------------------
Getter Method
Signature
AcrossVoids
Returns: Return type: NXOpen.CAM.AcrossVoids
New in version NX6.0.0.
License requirements: None.
ActionWhenGouging¶
-
MillCutParameters.
ActionWhenGouging
¶ Returns or sets the action when gouging
-------------------------------------
Getter Method
Signature
ActionWhenGouging
Returns: the When Gouging Check value Return type: NXOpen.CAM.CutParametersActionWhenGougingTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ActionWhenGouging
Parameters: propValue ( NXOpen.CAM.CutParametersActionWhenGougingTypes
) – the When Gouging Check valueNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
AdjacentBlades¶
-
MillCutParameters.
AdjacentBlades
¶ Returns or sets the Adjacent Blades Stock Option Type
-------------------------------------
Getter Method
Signature
AdjacentBlades
Returns: the adjacent blades stock option type Return type: NXOpen.CAM.CutParametersAdjacentBladesTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdjacentBlades
Parameters: adjacentBlades ( NXOpen.CAM.CutParametersAdjacentBladesTypes
) – the adjacent blades stock option typeNew in version NX8.5.0.
License requirements: cam_base (“CAM BASE”)
AllowUndercutting¶
-
MillCutParameters.
AllowUndercutting
¶ Returns or sets the allow undercutting toggle
-------------------------------------
Getter Method
Signature
AllowUndercutting
Returns: the Undercut Handle Flag Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AllowUndercutting
Parameters: propValue (bool) – the Undercut Handle Flag New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
ApplyToLastPass¶
-
MillCutParameters.
ApplyToLastPass
¶ Returns or sets the status for doing Blank Sensitive finish on the last cut level
-------------------------------------
Getter Method
Signature
ApplyToLastPass
Returns: apply to last pass status Return type: bool New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ApplyToLastPass
Parameters: applyLastPassStatus (bool) – apply to last pass status New in version NX7.5.1.
License requirements: cam_base (“CAM BASE”)
BladeStock¶
-
MillCutParameters.
BladeStock
¶ Returns the blade stock
-------------------------------------
Getter Method
Signature
BladeStock
Returns: the blade stock builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.0.0.
License requirements: None.
BlankDistance¶
-
MillCutParameters.
BlankDistance
¶ Returns the blank distance
-------------------------------------
Getter Method
Signature
BlankDistance
Returns: the blank distance builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
BlankOverhang¶
-
MillCutParameters.
BlankOverhang
¶ Returns the blank overhang (inheritable tool dependent).
Its relative UI name is changed to “Tool Overhang” from NX8.0. But it is named to “First Pass Overhang” in floor milling and floor and wall milling
-------------------------------------
Getter Method
Signature
BlankOverhang
Returns: the blank overhang Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX6.0.0.
License requirements: None.
BlankStock¶
-
MillCutParameters.
BlankStock
¶ Returns the blank stock
-------------------------------------
Getter Method
Signature
BlankStock
Returns: the stock blank builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
BlendStock¶
-
MillCutParameters.
BlendStock
¶ Returns the blend stock
-------------------------------------
Getter Method
Signature
BlendStock
Returns: the blend stock builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.0.0.
License requirements: None.
BoundaryApproximation¶
-
MillCutParameters.
BoundaryApproximation
¶ Returns or sets the boundary approximation toggle
-------------------------------------
Getter Method
Signature
BoundaryApproximation
Returns: the Boundary Profile Pass Flag Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundaryApproximation
Parameters: propValue (bool) – the Boundary Profile Pass Flag New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
BoundaryInTol¶
-
MillCutParameters.
BoundaryInTol
¶ Returns or sets the boundary intol
-------------------------------------
Getter Method
Signature
BoundaryInTol
Returns: the boundary intol value Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundaryInTol
Parameters: propValue (float) – the boundary intol value New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
BoundaryOutTol¶
-
MillCutParameters.
BoundaryOutTol
¶ Returns or sets the boundary out tol
-------------------------------------
Getter Method
Signature
BoundaryOutTol
Returns: the boundary out tol value Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundaryOutTol
Parameters: propValue (float) – the boundary out tol value New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
BoundaryStock¶
-
MillCutParameters.
BoundaryStock
¶ Returns or sets the boundary stock
-------------------------------------
Getter Method
Signature
BoundaryStock
Returns: the boundary stock value Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundaryStock
Parameters: propValue (float) – the trim stock value New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
CheckStock¶
-
MillCutParameters.
CheckStock
¶ Returns the check stock
-------------------------------------
Getter Method
Signature
CheckStock
Returns: The check stock builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
CleanupOutput¶
-
MillCutParameters.
CleanupOutput
¶ Returns the Cleanup Output
-------------------------------------
Getter Method
Signature
CleanupOutput
Returns: Return type: NXOpen.CAM.CleanupOutput
New in version NX6.0.0.
License requirements: None.
CleanupSettings¶
-
MillCutParameters.
CleanupSettings
¶ Returns the Cleanup Settings
-------------------------------------
Getter Method
Signature
CleanupSettings
Returns: Return type: NXOpen.CAM.CleanupSettings
New in version NX6.0.0.
License requirements: None.
CornerControl¶
-
MillCutParameters.
CornerControl
¶ Returns the corner control
-------------------------------------
Getter Method
Signature
CornerControl
Returns: Return type: NXOpen.CAM.CornerControlBuilder
New in version NX6.0.0.
License requirements: None.
CornerFindingOptions¶
-
MillCutParameters.
CornerFindingOptions
¶ Returns or sets the Corner Finding Options
-------------------------------------
Getter Method
Signature
CornerFindingOptions
Returns: the Finding Corner type Return type: NXOpen.CAM.CutParametersCornerFindingTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CornerFindingOptions
Parameters: cornerFinding ( NXOpen.CAM.CutParametersCornerFindingTypes
) – the Finding Corner typeNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
CutAngle¶
-
MillCutParameters.
CutAngle
¶ Returns the cut angle
-------------------------------------
Getter Method
Signature
CutAngle
Returns: Return type: NXOpen.CAM.CutAngle
New in version NX6.0.0.
License requirements: None.
CutAreaExtensionDistance¶
-
MillCutParameters.
CutAreaExtensionDistance
¶ Returns the cut area extension distance builder
-------------------------------------
Getter Method
Signature
CutAreaExtensionDistance
Returns: the cut area extension distance builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX6.0.0.
License requirements: None.
CutBelowOverhangingBlank¶
-
MillCutParameters.
CutBelowOverhangingBlank
¶ Returns or sets the Cut Below Overhanging Blank Method
-------------------------------------
Getter Method
Signature
CutBelowOverhangingBlank
Returns: Return type: bool New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
CutBelowOverhangingBlank
Parameters: propValue (bool) – the Cut Below Overhanging Blank Method New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
CutBelowToolContact¶
-
MillCutParameters.
CutBelowToolContact
¶ Returns or sets the cut below tool contact setting
-------------------------------------
Getter Method
Signature
CutBelowToolContact
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutBelowToolContact
Parameters: cutBelowToolContact (bool) – New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
CutBetweenLevels¶
-
MillCutParameters.
CutBetweenLevels
¶ Returns or sets the cut between levels
-------------------------------------
Getter Method
Signature
CutBetweenLevels
Returns: the cut between method Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutBetweenLevels
Parameters: cutBetween (bool) – the cut between method New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
CutDirection¶
-
MillCutParameters.
CutDirection
¶ Returns the cut direction
-------------------------------------
Getter Method
Signature
CutDirection
Returns: Return type: NXOpen.CAM.CutDirection
New in version NX6.0.0.
License requirements: None.
CutOrder¶
-
MillCutParameters.
CutOrder
¶ Returns or sets the cut order
-------------------------------------
Getter Method
Signature
CutOrder
Returns: Return type: NXOpen.CAM.CutParametersCutOrderTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutOrder
Parameters: propValue ( NXOpen.CAM.CutParametersCutOrderTypes
) –New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
CutWallsOnly¶
-
MillCutParameters.
CutWallsOnly
¶ Returns or sets the Cut Walls Only toggle
-------------------------------------
Getter Method
Signature
CutWallsOnly
Returns: the Cut Walls Only Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutWallsOnly
Parameters: propValue (bool) – the Cut Walls Only New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
ExtendAcrossUndercut¶
-
MillCutParameters.
ExtendAcrossUndercut
¶ Returns or sets the extend across undercut toggle
-------------------------------------
Getter Method
Signature
ExtendAcrossUndercut
Returns: the Extend Across Undercut value Return type: bool New in version NX10.0.2.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
ExtendAcrossUndercut
Parameters: propValue (bool) – the Extend Across Undercut value New in version NX10.0.2.
License requirements: cam_base (“CAM BASE”)
ExtendAtEdges¶
-
MillCutParameters.
ExtendAtEdges
¶ Returns the Extend At Edges
-------------------------------------
Getter Method
Signature
ExtendAtEdges
Returns: Return type: NXOpen.CAM.ExtendAtEdges
New in version NX6.0.0.
License requirements: None.
ExtendFloorTo¶
-
MillCutParameters.
ExtendFloorTo
¶ Returns or sets the extend floor to
-------------------------------------
Getter Method
Signature
ExtendFloorTo
Returns: the extend floor to option Return type: NXOpen.CAM.CutParametersExtendFloorTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtendFloorTo
Parameters: option ( NXOpen.CAM.CutParametersExtendFloorTypes
) – the extend floor to optionNew in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
ExtendToPart¶
-
MillCutParameters.
ExtendToPart
¶ Returns or sets the extend to part flag
-------------------------------------
Getter Method
Signature
ExtendToPart
Returns: the extend to part flag Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtendToPart
Parameters: flag (bool) – the extend to part flag New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
FinishPasses¶
-
MillCutParameters.
FinishPasses
¶ Returns the finish passes
-------------------------------------
Getter Method
Signature
FinishPasses
Returns: the finish passes builder Return type: NXOpen.CAM.FinishPassesBuilder
New in version NX6.0.0.
License requirements: None.
FloorSameAsPartStock¶
-
MillCutParameters.
FloorSameAsPartStock
¶ Returns or sets the floor same as part stock
-------------------------------------
Getter Method
Signature
FloorSameAsPartStock
Returns: the stock part use status Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FloorSameAsPartStock
Parameters: stockPartStatus (bool) – the stock part use status New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
FloorStock¶
-
MillCutParameters.
FloorStock
¶ Returns the floor stock
-------------------------------------
Getter Method
Signature
FloorStock
Returns: the floor stock builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
FollowCheck¶
-
MillCutParameters.
FollowCheck
¶ Returns or sets the follow check geometry status
-------------------------------------
Getter Method
Signature
FollowCheck
Returns: the Follow Check Geometry Status Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FollowCheck
Parameters: propValue (bool) – the Follow Check Geometry Status New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
FromLeadingEdge¶
-
MillCutParameters.
FromLeadingEdge
¶ Returns the from leading edge
-------------------------------------
Getter Method
Signature
FromLeadingEdge
Returns: Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX7.0.0.
License requirements: None.
FromTrailingEdge¶
-
MillCutParameters.
FromTrailingEdge
¶ Returns the from trailing edge
-------------------------------------
Getter Method
Signature
FromTrailingEdge
Returns: Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX7.0.0.
License requirements: None.
GlobalOptimization¶
-
MillCutParameters.
GlobalOptimization
¶ Returns or sets the global optimzation status
-------------------------------------
Getter Method
Signature
GlobalOptimization
Returns: global optimization status Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GlobalOptimization
Parameters: globalOptStatus (bool) – global optimization status New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
HubStock¶
-
MillCutParameters.
HubStock
¶ Returns the hub stock
-------------------------------------
Getter Method
Signature
HubStock
Returns: the hub stock builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.0.0.
License requirements: None.
IncludeBodiesOfSurfaceRegion¶
-
MillCutParameters.
IncludeBodiesOfSurfaceRegion
¶ Returns or sets the flag to check bodies of surface region
-------------------------------------
Getter Method
Signature
IncludeBodiesOfSurfaceRegion
Returns: flag of including bodies of surface region Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IncludeBodiesOfSurfaceRegion
Parameters: includeBodies (bool) – flag of including bodies of surface region New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
LevelToLevel¶
-
MillCutParameters.
LevelToLevel
¶ Returns the Level to Level
-------------------------------------
Getter Method
Signature
LevelToLevel
Returns: Return type: NXOpen.CAM.LevelToLevel
New in version NX6.0.0.
License requirements: None.
LowerLimit¶
-
MillCutParameters.
LowerLimit
¶ Returns the lower limit
-------------------------------------
Getter Method
Signature
LowerLimit
Returns: Return type: NXOpen.CAM.LowerLimit
New in version NX6.0.0.
License requirements: None.
MaxCutStep¶
-
MillCutParameters.
MaxCutStep
¶ Returns the maximum cut step
-------------------------------------
Getter Method
Signature
MaxCutStep
Returns: The Max. Step Size builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX6.0.0.
License requirements: None.
MaxCutTraverse¶
-
MillCutParameters.
MaxCutTraverse
¶ Returns the max cut traverse
-------------------------------------
Getter Method
Signature
MaxCutTraverse
Returns: Return type: NXOpen.CAM.MaxCutTraverse
New in version NX6.0.0.
License requirements: None.
MergeDistance¶
-
MillCutParameters.
MergeDistance
¶ Returns the merge distance builder (tool dependent double)
-------------------------------------
Getter Method
Signature
MergeDistance
Returns: Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX6.0.0.
License requirements: None.
MinCutVolume¶
-
MillCutParameters.
MinCutVolume
¶ Returns the minimum cut volume
-------------------------------------
Getter Method
Signature
MinCutVolume
Returns: Return type: NXOpen.CAM.MinCutVolume
New in version NX6.0.0.
License requirements: None.
MinMaterialThickness¶
-
MillCutParameters.
MinMaterialThickness
¶ Returns the minimum material thickness
-------------------------------------
Getter Method
Signature
MinMaterialThickness
Returns: the minimum thickness builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
MinimizeNumberOfEngages¶
-
MillCutParameters.
MinimizeNumberOfEngages
¶ Returns or sets the minimize number of engages toggle
-------------------------------------
Getter Method
Signature
MinimizeNumberOfEngages
Returns: the Minimize Number of Engages Flag Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinimizeNumberOfEngages
Parameters: propValue (bool) – the Minimize Number of Engages Flag New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
MultiDepthCut¶
-
MillCutParameters.
MultiDepthCut
¶ Returns the Multi Depth Cut
-------------------------------------
Getter Method
Signature
MultiDepthCut
Returns: Return type: NXOpen.CAM.MultiDepthCut
New in version NX6.0.0.
License requirements: None.
OutputUncutRegions¶
-
MillCutParameters.
OutputUncutRegions
¶ Returns the output uncut regions
-------------------------------------
Getter Method
Signature
OutputUncutRegions
Returns: Return type: NXOpen.CAM.OutputUncutRegions
New in version NX6.0.0.
License requirements: None.
PartStockOffset¶
-
MillCutParameters.
PartStockOffset
¶ Returns the part stock offset
-------------------------------------
Getter Method
Signature
PartStockOffset
Returns: The Part Stock Offset builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
PatternDirection¶
-
MillCutParameters.
PatternDirection
¶ Returns or sets the pattern direction
-------------------------------------
Getter Method
Signature
PatternDirection
Returns: Return type: NXOpen.CAM.CutParametersPatternDirectionTypes
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
PatternDirection
Parameters: propValue ( NXOpen.CAM.CutParametersPatternDirectionTypes
) –New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
PlungeDirection¶
-
MillCutParameters.
PlungeDirection
¶ Returns or sets the plunge direction
-------------------------------------
Getter Method
Signature
PlungeDirection
Returns: The plunge direction Return type: NXOpen.CAM.CutParametersPlungeDirectionTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlungeDirection
Parameters: propValue ( NXOpen.CAM.CutParametersPlungeDirectionTypes
) – The plunge directionNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
PreventUndercutting¶
-
MillCutParameters.
PreventUndercutting
¶ Returns or sets the prevent undercutting toggle
This property is deprecated. Use
NXOpen.CAM.MillCutParameters.AllowUndercutting`()
instead.-------------------------------------
Getter Method
Signature
PreventUndercutting
Returns: the Undercut Handle Flag Return type: bool New in version NX6.0.0.
Deprecated since version NX8.0.0: Use
NXOpen.CAM.MillCutParameters.AllowUndercutting`()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
PreventUndercutting
Parameters: propValue (bool) – the Undercut Handle Flag New in version NX6.0.0.
Deprecated since version NX8.0.0: Use
NXOpen.CAM.MillCutParameters.AllowUndercutting`()
instead.License requirements: cam_base (“CAM BASE”)
RegionConnection¶
-
MillCutParameters.
RegionConnection
¶ Returns or sets the region connection
-------------------------------------
Getter Method
Signature
RegionConnection
Returns: the Region Connection Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RegionConnection
Parameters: propValue (bool) – the Region Connection New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
RegionSequencing¶
-
MillCutParameters.
RegionSequencing
¶ Returns or sets the region resequencing
-------------------------------------
Getter Method
Signature
RegionSequencing
Returns: Return type: NXOpen.CAM.CutParametersRegionSequencingTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RegionSequencing
Parameters: propValue ( NXOpen.CAM.CutParametersRegionSequencingTypes
) –New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
RollToolOverEdges¶
-
MillCutParameters.
RollToolOverEdges
¶ Returns or sets the roll tool over edges toggle
-------------------------------------
Getter Method
Signature
RollToolOverEdges
Returns: the Remove Edge Traces value Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RollToolOverEdges
Parameters: propValue (bool) – the Remove Edge Traces value New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
RotaryMaxAngleLimit¶
-
MillCutParameters.
RotaryMaxAngleLimit
¶ Returns or sets the rotary max angle limit
-------------------------------------
Getter Method
Signature
RotaryMaxAngleLimit
Returns: the rotary max angle limit Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotaryMaxAngleLimit
Parameters: angle (float) – the rotary max angle limit New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
RotaryMinAngleLimit¶
-
MillCutParameters.
RotaryMinAngleLimit
¶ Returns or sets the min angle from part axis
-------------------------------------
Getter Method
Signature
RotaryMinAngleLimit
Returns: the rotary min angle limit Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotaryMinAngleLimit
Parameters: angle (float) – the rotary min angle limit New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
SelfIntersection¶
-
MillCutParameters.
SelfIntersection
¶ Returns or sets the Standard Drive Self-Intersect Status
-------------------------------------
Getter Method
Signature
SelfIntersection
Returns: The Standard Drive Self-Intersect Status value Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelfIntersection
Parameters: selfIntersect (bool) – The Standard Drive Self-Intersect Status value New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
ShroudStock¶
-
MillCutParameters.
ShroudStock
¶ Returns the shroud stock
-------------------------------------
Getter Method
Signature
ShroudStock
Returns: the shroud stock builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.0.0.
License requirements: None.
SimplifyShapes¶
-
MillCutParameters.
SimplifyShapes
¶ Returns or sets the Simplify Shapes Method
-------------------------------------
Getter Method
Signature
SimplifyShapes
Returns: Return type: NXOpen.CAM.CutParametersSimplifyShapesTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SimplifyShapes
Parameters: propValue ( NXOpen.CAM.CutParametersSimplifyShapesTypes
) –New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
SinglePassOffset¶
-
MillCutParameters.
SinglePassOffset
¶ Returns the Single Pass Offset
-------------------------------------
Getter Method
Signature
SinglePassOffset
Returns: Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX8.0.0.
License requirements: None.
SmallAreaAvoidance¶
-
MillCutParameters.
SmallAreaAvoidance
¶ Returns the small area avoidance
-------------------------------------
Getter Method
Signature
SmallAreaAvoidance
Returns: the small area builder Return type: NXOpen.CAM.SmallAreaAvoidance
New in version NX6.0.0.
License requirements: None.
SteepContainment¶
-
MillCutParameters.
SteepContainment
¶ Returns the steep containment
-------------------------------------
Getter Method
Signature
SteepContainment
Returns: Return type: NXOpen.CAM.SteepContainment
New in version NX6.0.0.
License requirements: None.
Stepover¶
-
MillCutParameters.
Stepover
¶ Returns the stepover
-------------------------------------
Getter Method
Signature
Stepover
Returns: Return type: NXOpen.CAM.StepoverBuilder
New in version NX6.0.0.
License requirements: None.
StepoverLimit¶
-
MillCutParameters.
StepoverLimit
¶ Returns the Stepover Limit
-------------------------------------
Getter Method
Signature
StepoverLimit
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
TextDepth¶
-
MillCutParameters.
TextDepth
¶ Returns the Text Depth
-------------------------------------
Getter Method
Signature
TextDepth
Returns: The Text Depth builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
TlaxisBladeRollAngle¶
-
MillCutParameters.
TlaxisBladeRollAngle
¶ Returns or sets the max blade roll angle
-------------------------------------
Getter Method
Signature
TlaxisBladeRollAngle
Returns: the max blade roll angle value Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TlaxisBladeRollAngle
Parameters: angle (float) – the max blade roll angle value New in version NX7.0.0.
License requirements: cam_base (“CAM BASE”)
TolerantMachining¶
-
MillCutParameters.
TolerantMachining
¶ Returns or sets the tolerant machining status
-------------------------------------
Getter Method
Signature
TolerantMachining
Returns: the tolerant machining status Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TolerantMachining
Parameters: tolerantMachine (bool) – the tolerant machining status New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
ToolAxisChange¶
-
MillCutParameters.
ToolAxisChange
¶ Returns the tool axis change
-------------------------------------
Getter Method
Signature
ToolAxisChange
Returns: Return type: NXOpen.CAM.ToolAxisChange
New in version NX6.0.0.
License requirements: None.
ToolAxisSmoothing¶
-
MillCutParameters.
ToolAxisSmoothing
¶ Returns or sets the degree of tool axis smoothing
-------------------------------------
Getter Method
Signature
ToolAxisSmoothing
Returns: the Smoothing value Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolAxisSmoothing
Parameters: smoothing (int) – the Smoothing value New in version NX7.0.0.
License requirements: cam_base (“CAM BASE”)
ToolAxisTilt¶
-
MillCutParameters.
ToolAxisTilt
¶ Returns the tool axis tilt
-------------------------------------
Getter Method
Signature
ToolAxisTilt
Returns: the tool axis tilt builder Return type: NXOpen.CAM.ToolAxisTilt
New in version NX6.0.0.
License requirements: None.
ToolRunOff¶
-
MillCutParameters.
ToolRunOff
¶ Returns the Tool Run Off
-------------------------------------
Getter Method
Signature
ToolRunOff
Returns: Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX8.0.0.
License requirements: None.
ToolRunOffType¶
-
MillCutParameters.
ToolRunOffType
¶ Returns or sets the Tool Run Off Type
-------------------------------------
Getter Method
Signature
ToolRunOffType
Returns: the Tool Run Off type Return type: NXOpen.CAM.CutParametersToolRunOffTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolRunOffType
Parameters: toolRunOff ( NXOpen.CAM.CutParametersToolRunOffTypes
) – the Tool Run Off typeNew in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
ToolRunOn¶
-
MillCutParameters.
ToolRunOn
¶ Returns the Tool Run On
-------------------------------------
Getter Method
Signature
ToolRunOn
Returns: Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX8.0.0.
License requirements: None.
ToolpathSmoothing¶
-
MillCutParameters.
ToolpathSmoothing
¶ Returns or sets the degree of tool path smoothing
-------------------------------------
Getter Method
Signature
ToolpathSmoothing
Returns: the Smoothing value Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolpathSmoothing
Parameters: smoothing (int) – the Smoothing value New in version NX7.0.0.
License requirements: cam_base (“CAM BASE”)
TraverseOpenPasses¶
-
MillCutParameters.
TraverseOpenPasses
¶ Returns or sets the open passes
-------------------------------------
Getter Method
Signature
TraverseOpenPasses
Returns: Return type: NXOpen.CAM.CutParametersTraverseOpenPassesTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TraverseOpenPasses
Parameters: propValue ( NXOpen.CAM.CutParametersTraverseOpenPassesTypes
) –New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
TrimControl¶
-
MillCutParameters.
TrimControl
¶ Returns or sets the trim control method type
-------------------------------------
Getter Method
Signature
TrimControl
Returns: Return type: NXOpen.CAM.CutParametersTrimControlTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrimControl
Parameters: propValue ( NXOpen.CAM.CutParametersTrimControlTypes
) –New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
TrimStock¶
-
MillCutParameters.
TrimStock
¶ Returns the trim stock
-------------------------------------
Getter Method
Signature
TrimStock
Returns: the Stock of Trim Geometry builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
TrochoidalSettings¶
-
MillCutParameters.
TrochoidalSettings
¶ Returns the Trochoidal Settings
-------------------------------------
Getter Method
Signature
TrochoidalSettings
Returns: Return type: NXOpen.CAM.TrochoidalSettings
New in version NX6.0.0.
License requirements: None.
UpDownCutting¶
-
MillCutParameters.
UpDownCutting
¶ Returns the up down cutting
-------------------------------------
Getter Method
Signature
UpDownCutting
Returns: Return type: NXOpen.CAM.UpDownCutting
New in version NX6.0.0.
License requirements: None.
UsePrevious2dIpw¶
-
MillCutParameters.
UsePrevious2dIpw
¶ Returns or sets the use previous IPW toggle
-------------------------------------
Getter Method
Signature
UsePrevious2dIpw
Returns: the Use Previous IPW Flag Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UsePrevious2dIpw
Parameters: propValue (bool) – the Use Previous IPW Flag New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
ValleyOverlapDistance¶
-
MillCutParameters.
ValleyOverlapDistance
¶ Returns the valley overlap distance
-------------------------------------
Getter Method
Signature
ValleyOverlapDistance
Returns: the valley overlap distance Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
WallStock¶
-
MillCutParameters.
WallStock
¶ Returns the wall stock
-------------------------------------
Getter Method
Signature
WallStock
Returns: the stock wall builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
ZAxisSmoothing¶
-
MillCutParameters.
ZAxisSmoothing
¶ Returns the Z Axis Smoothing.
-------------------------------------
Getter Method
Signature
ZAxisSmoothing
Returns: Return type: NXOpen.CAM.ZAxisSmoothing
New in version NX7.5.0.
License requirements: None.