LowerLimit Class¶
-
class
NXOpen.CAM.
LowerLimit
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.CAM.LowerLimit
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Action | Returns or sets the Lower Limit Action |
Mode | Returns or sets the Lower Limit Mode |
Plane | Returns or sets the Lower Limit Plane |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
LowerLimitActionTypes Enumeration | Available types for Lower Limit Actions |
LowerLimitModeTypes Enumeration | Available types for Lower Limit Mode |
Property Detail¶
Action¶
-
LowerLimit.
Action
¶ Returns or sets the Lower Limit Action
-------------------------------------
Getter Method
Signature
Action
Returns: The Lower Limit Actions value Return type: NXOpen.CAM.LowerLimitActionTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Action
Parameters: action ( NXOpen.CAM.LowerLimitActionTypes
) – lower limit action valueNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Mode¶
-
LowerLimit.
Mode
¶ Returns or sets the Lower Limit Mode
-------------------------------------
Getter Method
Signature
Mode
Returns: The Lower Limit Mode value Return type: NXOpen.CAM.LowerLimitModeTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Mode
Parameters: mode ( NXOpen.CAM.LowerLimitModeTypes
) – lower limit mode valueNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Plane¶
-
LowerLimit.
Plane
¶ Returns or sets the Lower Limit Plane
-------------------------------------
Getter Method
Signature
Plane
Returns: lower limit plane, entity type can be XFORM and PLANE Return type: NXOpen.NXObject
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Plane
Parameters: plane ( NXOpen.NXObject
) – lower limit plane, entity type can be XFORM and PLANENew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)