InheritableToolDepBuilder Class¶
-
class
NXOpen.CAM.
InheritableToolDepBuilder
¶ Bases:
NXOpen.CAM.InheritableDoubleBuilder
Represents a builder for an inheritable tool dependent value in of a CAM.
CAMObject .. versionadded:: NX5.0.0
Properties¶
Property | Description |
---|---|
InheritanceStatus | Returns or sets the inheritance status |
Intent | Returns or sets the current source setting |
Tag | Returns the Tag for this object. |
Value | Returns or sets the current value |
Methods¶
Property Detail¶
Intent¶
-
InheritableToolDepBuilder.
Intent
¶ Returns or sets the current source setting
-------------------------------------
Getter Method
Signature
Intent
Returns: the current source Return type: NXOpen.CAM.ParamValueIntent
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Intent
Parameters: newIntent ( NXOpen.CAM.ParamValueIntent
) – the new sourceNew in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)