FinishPassesBuilder Class¶
-
class
NXOpen.CAM.
FinishPassesBuilder
¶ Bases:
NXOpen.TaggedObject
Represents a FinishPasses Builder
This is an abstract class, and cannot be instantiated.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
FinishStepoverBuilder | Returns the parameter to define the stepover value for a finish pass |
NumberOfFinishPasses | Returns or sets the parameter to define number of finish passes |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
FinishStepoverBuilder¶
-
FinishPassesBuilder.
FinishStepoverBuilder
¶ Returns the parameter to define the stepover value for a finish pass
-------------------------------------
Getter Method
Signature
FinishStepoverBuilder
Returns: the finish stepover builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
NumberOfFinishPasses¶
-
FinishPassesBuilder.
NumberOfFinishPasses
¶ Returns or sets the parameter to define number of finish passes
-------------------------------------
Getter Method
Signature
NumberOfFinishPasses
Returns: Return type: int New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
NumberOfFinishPasses
Parameters: newValue (int) – New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)