CutAngle Class¶
-
class
NXOpen.CAM.
CutAngle
¶ Bases:
NXOpen.TaggedObject
Represents a boundary cut angle ci Builder
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
Type | Returns or sets the cut angle type |
Value | Returns or sets the cut angle value |
Vector | Returns or sets the single cut vector and two way vector |
Methods¶
Enumerations¶
CutAngleTypes Enumeration | Available types for cut angle type in boundary cut angle customizable item |
Property Detail¶
Type¶
-
CutAngle.
Type
¶ Returns or sets the cut angle type
-------------------------------------
Getter Method
Signature
Type
Returns: the Cut Angle Type Return type: NXOpen.CAM.CutAngleTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: cutAngType ( NXOpen.CAM.CutAngleTypes
) – the Cut Angle TypeNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Value¶
-
CutAngle.
Value
¶ Returns or sets the cut angle value
-------------------------------------
Getter Method
Signature
Value
Returns: the Cut Angle Value Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Value
Parameters: cutAng (float) – the Cut Angle Value New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Vector¶
-
CutAngle.
Vector
¶ Returns or sets the single cut vector and two way vector
-------------------------------------
Getter Method
Signature
Vector
Returns: the Cut Vector Return type: NXOpen.Direction
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vector
Parameters: vector ( NXOpen.Direction
) – the Cut VectorNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)