CutAngleTypes Enumeration¶
NXOpen.CAM.CutAngle.Types is an alias for NXOpen.CAM.CutAngleTypes
-
class
NXOpen.CAM.
CutAngleTypes
¶ Bases:
object
Available types for cut angle type in boundary cut angle customizable item
Enum Members
Enum Member Enum Member Description Auto Automatic Specify User Defined LongestLine Longest Line Vector Vector TwoWayVector Two Way Vector -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-