LevelToLevel Class¶
-
class
NXOpen.CAM.
LevelToLevel
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.CAM.LevelToLevel
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
RampAngle | Returns the ramp angle |
Tag | Returns the Tag for this object. |
Type | Returns or sets the level to level type |
Methods¶
Enumerations¶
LevelToLevelTypes Enumeration | Available types for level to level method |
Property Detail¶
RampAngle¶
-
LevelToLevel.
RampAngle
¶ Returns the ramp angle
-------------------------------------
Getter Method
Signature
RampAngle
Returns: the ramp angle builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
Type¶
-
LevelToLevel.
Type
¶ Returns or sets the level to level type
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.CAM.LevelToLevelTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: propValue ( NXOpen.CAM.LevelToLevelTypes
) –New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)