LevelToLevelTypes Enumeration¶
NXOpen.CAM.LevelToLevel.Types is an alias for NXOpen.CAM.LevelToLevelTypes
-
class
NXOpen.CAM.
LevelToLevelTypes
¶ Bases:
object
Available types for level to level method
Enum Members
Enum Member Enum Member Description UseTransferMethod Use transfer method DirectOnPart Direct on part RampOnPart Ramp on part StaggerRampOnPart Staggered ramp on part -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-